Skip to main content

10.4 External communication

10.4.1 Overview

The xCore system provides a Tcp Socket-based external communication interface supporting both server and client through which host systems (PLC, MES, etc.) can send control commands to the robot or obtain the robot status.

10.4.2 Configurations

Before using the interactive commands, configure the parameters related to the Socket communication and enable the function. The configuration interface is located in HMI →"Communication" → "External Communication", as shown in the following figure:

image539
image540

Note:

The Socket communication interface supports the robot to serve as a client or server, but only one state at a time.

When the robot is used as a client, the following parameters need to be configured:

Parameters Explanation

IP

Server IP, such as the IP address of the connected PLM and MES systems.

Port

Server-side listening port

Suffix

When the server sends control or monitoring commands to the robot, an additional suffix character is required at the end of the command. They are typically simple terminators such as \r, \n, or \t. Please note that combined suffixes can be used here without limitation on length, such as \r\n, \r\t, or \r\n\t. Visible characters such as letters can also be used.

The robot used as a server supports multiple connections. In this case, please pay attention to the control sequence on the client side to avoid any conflict. The following parameters need to be configured:

Parameters Explanation

Port

Server-side listening port

Suffix

When the server sends control or monitoring commands to the robot, an additional suffix character is required at the end of the command. They are typically simple terminators such as \r, \n, or \t. Please note that combined suffixes can be used here without limitation on length, such as \r\n, \r\t, or \r\n\t. Visible characters such as letters can also be used.

10.4.3 Interactive commands

Interactive commands include control commands and monitoring commands.
The following table gives the specific command content and format. (Assuming the user uses "\r" as the specified command terminator, "\r" is an escape character representing carriage return, and the decimal value is 13).

Control commands:

Command name

String sent

Return value

Remarks

Close the socket interface

“xCore::SocketInterface::Disable” +“\r”

No return value

Start the socket interface

“xCore::SocketInterface::Enable” +“\r”

No return value

Start program

“start”+“\r”

"true" if success;
"false" if failed

It is not allowed to start the program through system IO when the register equipped with the pause function or system IO has not been reset;
After triggering the function code, if the teach pendant displays the alarm "Program not synchronized to controller, startup failed", synchronize the program and retrigger the function code;

Stop program

“stop”+“\r”

"true" if success;
"false" if failed

Clear servo alarms

“clear_alarm”+”\r”

"true" if success;
"false" if failed

Program pointer to main

“pp_to_main”+“\r”

"true" if success;
"false" if failed

Motor power-on

“motor_on”+“\r”

"true" if success;
"false" if failed

Motor power-off

“motor_off” + “\r”

"true" if success;
"false" if failed

Switch to Manual mode

“switch_mode:manual”+”\r”

"true" if success;
"false" if failed

Switch to Automatic mode

“switch_mode:auto”+”\r”

"true" if success;
"false" if failed

Enable Drag mode

“open_drag”+”\r”

"true" if success;
"false" if failed

Collaborative robot only

Disable Drag mode

“close_drag”+”\r”

"true" if success;
"false" if failed

Collaborative robot only

Obtain project list

list_prog + “\r”

Return to project list;
"null" if no project is returned

Obtain current project

current_prog + “\r”

Return to current load project;
"null" if no project is returned

Switch to project

load_prog + (project name) + "\r"

"true" if success;
"false" if failed

Set DO value

"setdo:" + "IO name, IO value" + "\r"

"true+r" if successful
"false+r" if not found

"setdo: DO0-0, true\r"
(pay attention to English punctuation)

Update the time on the controller and teach pendant

set_robot_time:time + "+r" (time format:Y YYY-MM-DD hh:mm:ss)

"true" if success;
"false" if failed

Emergency reset

estop_reset + “\r”

"true" if success;
"false" if failed

(RSC only, not applicable to mini board)

Emergency & clear alarm

estopreset_and_clearalarm +“\r”

"true" if success;
"false" if failed

Power on, program pointer to main, and start program in order

motoron_pptomain_start +“\r”

"true" if success;
"false" if failed

After triggering the function code, if the teach pendant displays the alarm "Program not synchronized to controller, startup failed", synchronize the program and retrigger the function code;

Power on and start program in order

motoron_start +“\r”

"true" if success;
"false" if failed

After triggering the function code, if the teach pendant displays the alarm "Program not synchronized to controller, startup failed", synchronize the program and retrigger the function code;

Pause program and power down in order

pause_motoroff +“\r”

"true" if success;
"false" if failed

Set program running rate

set_program_speed: +program speed +"\r"

"true" if success;
"false" if failed

Trigger and release robot soft E-stop

set_soft_estop:true/false +“\r”

"true" if success;
"false" if failed

Execute switch to automatic mode and then power on

switch_auto_motoron +“\r”

"true" if success;
"false" if failed

Open the corresponding safe region

open_safe_region: +safe region index+"\r"

"true" if success;
"false" if failed

Index range [1-10]

Close the corresponding safe region

close_safe_region: +safe region index+"\r"

"true" if success; "false" if failed

Index range [1-10]

Enable reduced mode

open_reduced_mode +“\r”

"true" if success;
"false" if failed

Disable reduced mode

close_reduced_mode +“\r”

"true" if success;
"false" if failed

Monitoring commands:

Command name

String sent

Return value

Remarks

Motor power state

“motor_on_state” + “\r”

"true" if success, motor power-on;
"false" if failed, motor power-off;

Program status

“robot_running_state” + “\r”

"true" if success, running;
"false" if failed, not running;

EStop state

“estop_state” + “\r”

When the emergency stop trigger level type is set to high: true, emergency stop; false, non-emergency stop.
When the emergency stop trigger level type is set to low: true, non-emergency stop; false, emergency stop.

The return value of this state is affected by the "Emergency Stop Trigger Level Type" setting. When it is set to high level, the output is valid when triggering a soft emergency stop, and invalid when not triggered; when it is set to low level, the output is invalid when triggering a soft emergency stop, and valid when not triggered.

Fault

“fault_state” + “\r”

"true" if success, fault;
"false" if failed, non-fault;

Operating mode

“operating_mode” + “\r”

"true" if success, automatic mode;
"false" if failed, manual mode/wait mode;

Get Cartesian position

“cart_pos” + “\r”

Cartesian position string + "\r";

Get Cartesian position

“cart_pos_name” + “\r”

"cart_pos: " + Cartesian position string + "\r";

Get axis position

“jnt_pos” + “\r”

Axis position string + "\r";

Get axis position

“jnt_pos_name” + “\r”

"jnt_pos: " + axis position string +"\r";

Get axis velocity

“jnt_vel” + “\r”

Axis speed string + "\r";

Unit: rad/s

Get axis velocity

“jnt_vel_name” + “\r”

"jnt_vel: "+ axis speed string + "\r";

Unit: rad/s

Get axis torque

“jnt_trq” + “\r”

Axis torque string + "\r";

Unit: N.m

Get axis torque

“jnt_trq_name” + “\r”

"jnt_trq:" + axis torque string + "\r";

Unit: N.m

Home state output

“home_state” + “\r”

"true" with output;
"false" without output

Collision detection state

“collision_state” + “\r”

"true" if trigger collision;
"false" if no collision

Collaborative robot only

Obtain robot task state

“task_state” + “\r”

The task currently performed by the robot. These include:
ready;
jog;
load_identify;
dynamic_identify;
drag;
program;
demo;
rci;
debug;

Please refer to the "HMI Introduction" for the icon and description of the current status of the robot

Obtain alarm state

“alarm_state”+”\r”

"true" if there is an alarm, "false" if no alarm is present

Obtain collision detection alarm state

“collision_alarm_state” + ”\r”

"true" if there is an alarm, "false" if no alarm is present

Obtain collision detection enable state

“collision_open_state” + ”\r”

"true" if collision detection is enabled
"false" if it is not enabled

Check if the controller is powered on

“controller_is_running”+ ”\r”

"true" if powered on
"false" if not powered on

Low-voltage alarm state of encoder

“encoder_low_battery_state”+ ”\r”

"true" if there is a low voltage alarm
"false" if there is no low voltage alarm

Obtain robot error code

“robot_error_code” + ”\r”

"robot error code" if an error is present
"0" if there is no error

Obtain pause state of RL

“program_full” + ”\r”

Pause state of RL, including:
0: initialization state;
1: RL running;
2: HMI paused;
3: system IO paused;
4: register function code paused;
5: external communication paused;
6: DK paused;
7: paused by Pause command;
10: emergency stop;
11. safety gate;
12. paused due to other factors.

Obtain program reset state

“program_reset_state”+ ”\r”

Output "true" if the program pointer is at the first line of the main function and the program has not started running; otherwise, output "false"

Obtain the actual speed of the current program execution

“program_speed” + “\r”

Actual speed of the current program execution Range: 1 to 100

Obtain program busy state

“robot_is_busy” + “\r”

"true" if currently in pptomain
Otherwise, "false"

Obtain whether the robot is executing time-consuming operations such as pptomain

Obtain whether the robot is in motion

“robot_is_moving” + ”\r”

"true" if the robot is moving
Otherwise, "false"

Obtain safety gate state

“safe_door_state” + ”\r”

"true" if safety gate is open
Otherwise, "false"

Obtain soft E-stop trigger status

“soft_estop_state” + ”\r”

"true" if the soft E-stop is triggered; otherwise, "false"

Obtain Cartesian velocity

“cart_vel” + “\r”

Cartesian velocity+"+r"

Obtain the pose of the robot’s TCP

“tcp_pose” + “\r”

Pose of the robot’s TCP+"\r"

Obtain the velocity of the robot’s TCP

“tcp_vel” + “\r”

Velocity of the robot’s TCP+"\r"

Obtain the composite linear velocity of the robot’s TCP

“tcp_vel_mag” + “\r”

Composite linear velocity of the robot’s TCP+"\r"

Obtain external E-stop state

“ext_estop_state” + “\r”

"true" if the external E-stop is triggered
"false" if it is not triggered

The safeboard is a mini board, and the firmware version is not less than 1.0.8.7

Obtain handheld E-stop state

“hand_estop_state” + “\r”

"true" if the handheld E-stop is triggered
"false" if non-handheld E-stop is triggered

The safeboard is a mini board, and the firmware version is not less than 1.0.8.7

Obtain collaboration mode state

“collaboration_state” + “\r”

"true" if collaboration mode is triggered
"false" if non-collaboration mode is triggered

Obtain reduced mode state

reduced_mode_state + “\r”

"true" if it is enabled; "false" if it is not enabled

Obtain IO state

io_state: + IO names (multiple IOs separated by commas) + "\r"

Return IO values as "true" or "false"; "null" if the corresponding IO is not found

On path verification

“sta_on_path” + “\r”

"true" if on path
"false" if off path

Refer to register function code "sta_on_path" for detailed usage

Near path point verification

“sta_near_path” + “\r”

"true" if near path point
"false" if not near path point

Refer to register function code "sta_near_path" for detailed usage

Obtain controller time

“get_robot_time”+“\r"

Return the current controller time. "false" if it failed

Drag status

”drag_state“ + “\r”

"true" if the drag switch is on
"false" if the drag switch is off

Only applicable for collaborative models

Status of drag button 1

”drag_button1“ + “\r”

"true" if the drag button 1 is pressed
"false" if the drag button 1 is not pressed

Only applicable for collaborative models

Status of drag button 2

”drag_button2“ + “\r”

"true" if the drag button 2 is pressed
"false" if the drag button 2 is not pressed

Only applicable for non-SR collaborative models; for CR models with only one drag button, "true" if either drag_button1 or drag_button2 is pressed

Obtain the resultant linear velocity of the TCP relative to the robot base frame

“tcp_ref_base_vel_mag”+ “\r”

Resultant linear velocity of the TCP relative to the robot base frame + "\r"

float type, in mm/s;

Obtain the resultant linear velocity of the TCP relative to the robot world frame

“tcp_ref_world_vel_mag”+ “\r”

Resultant linear velocity of the TCP relative to the robot world frame + "\r"

float, in mm/s;

Obtain the pose of the TCP relative to the robot base frame

“tcp_ref_base_pose”+ “\r”

Pose of the TCP relative to the robot base frame + "\r"

float array with a length of 7 (position in mm, quaternion)

Obtain the pose of the TCP relative to the robot world frame

“tcp_ref_world_pose“+ “\r”

Pose of the TCP relative to the robot world frame + "\r"

float array
with a length of 7 (position in mm, quaternion);

Obtain the robot joint position

“robot_jnt_pos“+ “\r”

Robot joint position + "\r"

float array
with a length of 7, in rad or mm;

Obtain the robot joint velocity

“robot_jnt_vel“+ “\r”

Robot joint velocity + "+r"

float array
with a length of 7, in rad/s or mm/s;

Obtain the robot joint torque

“robot_jnt_trq“+ “\r”

Robot joint torque + "\r"

float array
with a length of 7, in N.m;

Obtain additional axis joint position

“ext_jnt_pos“+ “\r”

Additional axis joint position + "\r"

float array
with a length of 6, in rad or mm;

Obtain additional axis joint velocity

“ext_jnt_vel“+ “\r”

Additional axis joint velocity + "\r"

float array
with a length of 6, in rad/s or mm/s;

Obtain additional axis joint torque

“ext_jnt_trq“+ “\r”

Additional axis joint torque + "\r"

float array
with a length of 7, in N.m;

Note:

String format

Unit

Cartesian position

x、y、z、a、b、c、q1、q2、q3、q4

x, y, and z in mm;
a, b, and c in degree;
Q1~q4 are orientation quaternions;

Axis position

j1、j2、j3、j4、j5、j6、j7

Robot axis angle in rad;
Additional axis position in m or rad;

Axis velocity

vj1、vj2、vj3、vj4、vj5、vj6、vj7

Robot velocity angle in rad/s;
Additional axis velocity in m/s or rad/s;

Axis torque

tj1、tj2、tj3、tj4、tj5、tj6、tj7

The unit of the robot axis and additional axis torque is the thousandth of the rated torque of the motor;