Skip to main content

Import and Use the Virtual Machine

Overview​

This image is a VMware virtual machine image. It provides a Linux environment for multi-platform plugin compilation and plugin packaging tools. You can use it to compile plugin source code, perform cross-platform builds, and generate plugin packages, improving consistency and convenience across development and delivery.

Download​

Download the virtual machine image file before importing it as described below.

Usage Steps​

1. Install VMware Workstation Pro​

Complete Install VMware first.

2. Import the Virtual Machine Image​

Open VMware Workstation Pro and drag the virtual machine image file into the main window to complete the import.

Import virtual machine image

After import, you can change the display name of the virtual machine in the list as needed.

Rename virtual machine image

3. Start and Sign In to the Virtual Machine​

After the virtual machine starts, sign in with the following account:

NameValue
Usernamerokae
Password123456

4. Plugin Project Directories​

After sign-in, plugin-related projects are located by default at:

/home/rokae/rokae/xplugin

Directory layout:

Directory nameDescription
clientHMI (client) plugins
controllerController plugins
electricclawpluginElectric gripper sample plugin (includes both HMI and controller sidesa full-stack engineering example with complete front-end and back-end interaction)

Plugin folder location

5. Plugin Compile and Package​

The image includes a plugin compile and packaging service that you can use to compile and package plugins. Open http://<VM-IP>:8008/ in a browser to access the service.