Environment Overview
Select a scenario based on the target artifact, then complete preparation according to the corresponding steps in the table.
| Development scenario | Environment setup steps |
|---|---|
| Client plugin (Windows) | 1. Secondary Dev Packages 2. Install MSVC 3. Install Qt 4. Configure Qt Creator |
| Client plugin (teach pendant Linux) | 1. Complete “Client plugin (Windows)” above (optional) 2. Secondary Dev Packages 3. Cross-Compilation Notes 4. Install VMware 5. Import and Use the Virtual Machine 6. Compile and Package Service |
| Controller plugin | 1. Secondary Dev Packages 2. Cross-Compilation Notes 3. Install VMware 4. Import and Use the Virtual Machine 5. Compile and Package Service |
tip
Step 1 of “Client plugin (teach pendant Linux)” is optional. To develop and verify on Windows first before use on the teach pendant, complete “Client plugin (Windows)” beforehand.