Skip to main content

Command Registration

This section describes how to register a command.

Command registration flow:

Command registration flow

Usage example:

/**
* @brief Command construction and registration
*/
void RegPrintq() {
// 1. Command configuration: name, trigger mode, task limits, etc.
RLCmdConfigAPI cfg;
cfg.SetFuncName("printq");
// Set look-ahead mode; default WAIT_MOVE_PAUSE
cfg.SetLookAhead(CmdLookAheadImplAPI::WAIT_MOVE_PAUSE) ;
// Set task limit type
cfg.SetTaskLimit(TaskLimitAPI::TASK_NO_LIMIT);
// Set step-back type
cfg.SetStepBack(StepBackAPI::STEP_BACK_SKIP);

// 2. Create command from configuration
BEGIN_COMMAND_API(cfg)

// 3. Configure parameter checkers for the command
PARAMS_API(
ArgTypeAPI(ValueTypeAPI::VALUE_ROBTARGET),
ArgTypeAPI(ValueTypeAPI::VALUE_WOBJ),
ArgTypeAPI(ValueTypeAPI::VALUE_STRING)
)

// 4. Forward execution body
RLCmdActionAPI cmd_func = [=](std::shared_ptr<RLCallFrameAPI> frame,
std::vector<std::shared_ptr<SymbolVarBaseAPI>> args) -> CommandExecuteAPI {
// Get nested data
auto cart_pos = args[0]->GetSubUnit("ROT");
std::vector<double> robs_q = {
cart_pos.GetSubUnit("Q1").GetDoubleVal(), cart_pos.GetSubUnit("Q2").GetDoubleVal(),
cart_pos.GetSubUnit("Q3").GetDoubleVal(), cart_pos.GetSubUnit("Q4").GetDoubleVal()};

CommandExecuteAPI cmd_exec = [=]()
{
LOG_INFO << "printq:" << frame->GetCmdTask() << " " << frame->GetCmdFile() << " " << frame->GetCmdLine();

LOG_INFO << "printq Q1=" << robs_q[0] << " Q2=" << robs_q[1] << " Q3=" << robs_q[2] << " Q4=" << robs_q[3] << " ";
LOG_INFO << "printq str=" << args[2]->GetStringVal();
return CommandProcessResultAPI::CMD_PROCESS_SUCCESS;
};
return cmd_exec;
};
EXECUTE_API(cmd_func)

// 5. Step-back execution body (add as needed)
RLCmdActionAPI cmd_func_stb = [=](std::shared_ptr<RLCallFrameAPI> frame,
std::vector<std::shared_ptr<SymbolVarBaseAPI>> args) -> CommandExecuteAPI {
// Get nested data
auto cart_pos = args[0]->GetSubUnit("ROT");

std::vector<double> robs_q = {
cart_pos.GetSubUnit("Q1").GetDoubleVal(), cart_pos.GetSubUnit("Q2").GetDoubleVal(),
cart_pos.GetSubUnit("Q3").GetDoubleVal(), cart_pos.GetSubUnit("Q4").GetDoubleVal()};

CommandExecuteAPI cmd_exec = [=]()
{
LOG_INFO << "printq:" << frame->GetCmdTask() << " " << frame->GetCmdFile() << " " << frame->GetCmdLine();

LOG_INFO << "printq Q1=" << robs_q[0] << " Q2=" << robs_q[1] << " Q3=" << robs_q[2] << " Q4=" << robs_q[3] << " ";
LOG_INFO << "printq str=" << args[2]->GetStringVal();
return CommandProcessResultAPI::CMD_PROCESS_SUCCESS;
};
return cmd_exec;
};
EXECUTE_STB_API(cmd_func_stb)

// 6. Register the command with the controller
REGISTER_COMMAND_API
}

When printq is used in the HMI, reaching that command prints the quaternion in the log. Users can inject the command through the client plugin in auxiliary programming for convenient use of newly registered commands.

HMI command usage

Command result

For a complete example, see examples/rl_cmd.hpp.

This command prints the quaternion of a Cartesian variable.