Creating the Plugin Package
Follow this format when creating the plugin package and configuration file so the package can be imported into Rokae+.
Package Structure
The HMI imports a plugin package (zip) that contains data packages:
- client.zip: client plugins
- controller.zip: controller plugins
The plugin package may include both, or only one of them. Client and controller plugins have no mandatory dependency on each other.
To deliver more than one plugin, use either approach:
- Separate packages: Build a separate plugin package (and its data packages) for each plugin, and import them individually.
- Combined package: Place multiple plugin directories side by side in the same client.zip or controller.zip, and import once.
The following sections describe both layouts.
1. One Plugin
Single-architecture package with both client and controller:
Package.zip # plugin package
├── client.zip # client data package
│ └── MyPlugin/
│ ├── MyPlugin.dll # Windows: .dll suffix; Linux: .so suffix
│ ├── xplugin.dll # framework library; Windows: .dll; Linux: .so
│ └── MyPlugin.json # configuration file
└── controller.zip # controller data package
└── MyPlugin/
├── MyPlugin.lic # license file
├── MyPlugin.so # controller binary (.so)
└── MyPlugin.json # configuration file
2. Multiple Plugins in One Data Package (Combined)
Place multiple plugin directories side by side in the same client.zip or controller.zip. Each directory holds one plugin and uses the same layout as a single-plugin package. One import installs all plugins in the package.
Example with both MyPlugin and OtherPlugin on client and controller:
Package.zip
├── client.zip
│ ├── MyPlugin/
│ │ ├── MyPlugin.dll # Windows: .dll suffix; Linux: .so suffix
│ │ ├── xplugin.dll # framework library; Windows: .dll; Linux: .so
│ │ └── MyPlugin.json # configuration file
│ └── OtherPlugin/
│ ├── OtherPlugin.dll # Windows: .dll suffix; Linux: .so suffix
│ ├── xplugin.dll # framework library; Windows: .dll; Linux: .so
│ └── OtherPlugin.json # configuration file
└── controller.zip
├── MyPlugin/
│ ├── MyPlugin.lic # license file
│ ├── MyPlugin.so # controller binary (.so)
│ └── MyPlugin.json # configuration file
└── OtherPlugin/
├── OtherPlugin.lic # license file
├── OtherPlugin.so # controller binary (.so)
└── OtherPlugin.json # configuration file
In the client configuration, depend lists client plugin dependencies and ctrlDepend lists controller plugin dependencies. In the controller configuration, depend lists other controller plugins that the plugin depends on.
Configuration File
Client Configuration File
Place MyPlugin.json in the plugin directory in client.zip.
{
"client_plugin": {
"name": "MyPlugin",
"depend": [],
"ctrlDepend": [],
"enable": false,
"version": "3.0.1",
"min_hmi_version": "3.0.1",
"custom_hmi_version": [],
"author": "rokae",
"description": "description"
}
}
Optional fields (marked ✗ in the table) may be omitted from the JSON file.
| Field | Required | Description |
|---|---|---|
| name | ✓ | Plugin name; naming rules are in Plugin Name Consistency below |
| depend | ✗ | Names of other client plugins this plugin depends on; use [] when none |
| ctrlDepend | ✗ | Names of controller plugins this plugin depends on |
| enable | ✓ | Whether the plugin is enabled by default after import; false in this example |
| version | ✓ | Plugin version |
| min_hmi_version | ✗ | Minimum supported HMI (xCore) version |
| custom_hmi_version | ✗ | Custom compatible version list |
| author | ✗ | Author |
| description | ✗ | Description |
Controller Configuration File
Place MyPlugin.json in the plugin directory in controller.zip. The top-level key is controller_plugin. The key under it, MyPlugin, must match name, the plugin directory name, and the configuration file's base name.
{
"controller_plugin": {
"MyPlugin": {
"name": "MyPlugin",
"depend": [],
"enable": true,
"min_controller_version": "3.0.2",
"must_controller_version": [],
"version": "1.0.0",
"author": "rokae",
"description": "description"
}
}
}
| Field | Required | Description |
|---|---|---|
| name | ✓ | Plugin name, following the rules in Plugin Name Consistency below |
| depend | If there are dependencies | Names of other controller plugins this plugin depends on, or [] if there are none |
| enable | ✓ | Whether the plugin is enabled by default after import (true to enable, false to disable and skip loading) |
| min_controller_version | ✗ | Minimum controller version required to run the plugin |
| must_controller_version | ✗ | Exact controller versions the plugin can run on, overriding min_controller_version when the list is non-empty ([] if unspecified) |
| version | ✗ | Plugin version |
| author | ✗ | Author |
| description | ✗ | Description |
Plugin Name Consistency
The plugin name in each of the following places must be the same string. Examples use MyPlugin; in a combined package, OtherPlugin follows the same rules with OtherPlugin throughout.
-
Project registration
PLUGIN_NAME in the Qt project and the KEY of XPLUGIN_REGISTER must beMyPlugin. -
Data-package directory and files
Paths and base file names for this plugin inside the plugin package must beMyPlugin:
Package.zip
├── client.zip
│ └── MyPlugin/ # deploy directory name = MyPlugin
│ ├── MyPlugin.dll # user plugin binary base name = MyPlugin (MyPlugin.so on Linux)
│ ├── xplugin.dll
│ └── MyPlugin.json # configuration file name = MyPlugin
└── controller.zip
└── MyPlugin/ # deploy directory name = MyPlugin
├── MyPlugin.lic # license file base name = MyPlugin
├── MyPlugin.so # controller binary base name = MyPlugin
└── MyPlugin.json # configuration file name = MyPlugin
-
name in the configuration file
The name field inMyPlugin.jsonmust be"MyPlugin". -
Dependency declarations (if any)
Names listed in depend / ctrlDepend must match the dependent plugin’s name in all items above (for example"OtherPlugin"when depending on OtherPlugin).
Quick Generation with Scripts
Scripts provided with this documentation pack prepared client / controller directories into an importable plugin package.
Get the Scripts
Place the following files in the same working directory as the client and controller directories:
| File | Description |
|---|---|
| PluginPackage.bat | Windows packaging script |
| PluginPackage.sh | Linux packaging script |
Prepare the Directory
Use the following layout (client-only or controller-only is allowed). Multiple plugin directories may be placed under client / controller:
Working directory/
├── client/ # optional
│ ├── MyPlugin/
│ │ ├── MyPlugin.dll # Windows: .dll suffix; Linux: .so suffix
│ │ ├── xplugin.dll # framework library; Windows: .dll; Linux: .so
│ │ └── MyPlugin.json # configuration file
│ └── OtherPlugin/ # optional
│ ├── OtherPlugin.dll # Windows: .dll suffix; Linux: .so suffix
│ ├── xplugin.dll # framework library; Windows: .dll; Linux: .so
│ └── OtherPlugin.json # configuration file
├── controller/ # optional
│ └── MyPlugin/
│ ├── MyPlugin.lic # license file
│ ├── MyPlugin.so # controller binary (.so)
│ └── MyPlugin.json # configuration file
└── PluginPackage.bat # or PluginPackage.sh
Generation Steps (Windows)
- Confirm that the working directory contains PluginPackage.bat, and client and/or controller.
- Double-click PluginPackage.bat.
- When the console reports completion, a plugin package zip is created in the same directory (default file name is the current folder name; rename if required).
- Import the zip in plugin management.
Output
Package.zip
├── client.zip # packed from client/
└── controller.zip # packed from controller/
- If only client is present, the plugin package contains only client.zip.
- If only controller is present, the plugin package contains only controller.zip.
FAQ
| Issue | Action |
|---|---|
| client / controller not found | Place the script in the same directory as those folders |
| Multi-architecture not as expected | Architecture directory names must be aarch64 / amd64 / win (controller has no win) |
Multi-Architecture Package
Rokae+ supports storing per-architecture data within one plugin package. Under client.zip / controller.zip, create architecture subdirectories first, then place the same plugin directory layout as for a single architecture.
- Client (client.zip): aarch64, amd64, win
- Controller (controller.zip): aarch64, amd64
Package.zip
├── client.zip
│ ├── aarch64
│ │ └── MyPlugin/
│ │ ├── MyPlugin.so
│ │ ├── xplugin.so
│ │ └── MyPlugin.json
│ ├── amd64
│ │ └── MyPlugin/
│ │ ├── MyPlugin.so
│ │ ├── xplugin.so
│ │ └── MyPlugin.json
│ └── win
│ └── MyPlugin/
│ ├── MyPlugin.dll
│ ├── xplugin.dll
│ └── MyPlugin.json
└── controller.zip
├── aarch64
│ └── MyPlugin/
│ ├── MyPlugin.lic
│ ├── MyPlugin.so
│ └── MyPlugin.json
└── amd64
└── MyPlugin/
├── MyPlugin.lic
├── MyPlugin.so
└── MyPlugin.json
Multi-architecture packages are supported since plugin 1.0.2.6, with xCore v3.2.2 or later.
Next Step
Import the plugin package in the HMI and enable it according to Installation and Usage.