Skip to main content

Custom Motion Commands

Call flow:

Motion command call flow

Example of implementing a custom motion command:

Step 1: set motion parameters.

Step 2: call SendCmd to send the command to the controller.

Implement command PMoveL(point,speed,zone,tool,wobj).

This command is similar to the existing MOVEL command. Users can implement custom logic inside the command, for example for welding applications.

/**
* @brief Implement PMoveL command
*/
void RegPMoveL() {
// 1. Command configuration: name, trigger mode, task limits, etc.
RLCmdConfigAPI cfg;
cfg.SetFuncName("pmovel");
// Set look-ahead mode to motion command
cfg.SetLookAhead(CmdLookAheadImplAPI::MOVEMENT_ITSELF) ;
// Set task limit type
cfg.SetTaskLimit(TaskLimitAPI::TASK_NO_LIMIT);
// Set step-back type
cfg.SetStepBack(StepBackAPI::STEP_BACK_CUSTOM);

// 2. Create command from configuration
BEGIN_COMMAND_API(cfg)

// 3. Configure parameter checkers for the command
PARAMS_API(
ArgTypeAPI(ValueTypeAPI::VALUE_ROBTARGET),
ArgTypeAPI(ValueTypeAPI::VALUE_SPEED),
ArgTypeAPI(ValueTypeAPI::VALUE_ZONE),
ArgTypeAPI(ValueTypeAPI::VALUE_TOOL),
ArgTypeAPI(ValueTypeAPI::VALUE_WOBJ)
)

// 4. Forward execution body
RLCmdActionAPI cmd_func = [=](std::shared_ptr<RLCallFrameAPI> frame,
std::vector<std::shared_ptr<SymbolVarBaseAPI>> args) -> CommandExecuteAPI {
// Get parameter data
auto point = args[0]->GetPointAPI();
auto speed = args[1]->GetSpeedAPI();
auto zone = args[2]->GetZoneAPI();
auto tool = args[3]->GetToolAPI();
auto wobj = args[4]->GetWobjAPI();

CommandExecuteAPI cmd_exec = [=]()
{
MotionCmdArgsAPI args_api;
// Set target point
args_api.SetTargetPoint(point);
// Set motion type to linear
args_api.SetMoveType(MoveTypeAPI::MOVE_L);
// Set tool, work object, speed, and zone
args_api.SetTool(tool);
args_api.SetWobj(wobj);
args_api.SetZone(zone);
args_api.SetSpeed(speed);
// Set pointer for current execution position
args_api.SetUpdatePointer(frame->GetCmdTask(), frame->GetCmdFile(), frame->GetCmdLine());
// Set trigger
TriggerAPI t;
t.type = TriggerAPI::TriggerType::DISTANCE;
t.reference_is_from_start = true;
t.value_from_reference = 0.1;
t.trigger_callback = [=]
{
LOG_DEBUG<<frame->GetCmdTask()<<" "<<frame->GetCmdFile()<<" "<<frame->GetCmdLine()<<" 100mm trigger callback";
};
args_api.SetTriggers({t});
// Set path callbacks
args_api.SetCallback(CallBackTypeAPI::MOVE_START,[]{LOG_INFO<<"movel start callback";});
args_api.SetCallback(CallBackTypeAPI::MOVE_FINISH,[]{LOG_INFO<<"movel finish callback";});
args_api.SetCallback(CallBackTypeAPI::MOVE_PAUSE,[]{LOG_INFO<<"movel pause callback";});
MotionCmdAPI api;
// Send command
int ret = api.SendCmd(args_api);
LOG_INFO<<"send motion cmd:"<<ret;
LOG_DEBUG<<"point:"<<point<<" speed:"<<speed<<" zone:"<<zone
<<" tool:"<<tool<<" wobj:"<<wobj;

LOG_DEBUG<<":"<<frame->GetCmdTask()<<" "<<frame->GetCmdFile()<<" "<<frame->GetCmdLine();
if (ret == 0){
return CommandProcessResultAPI::CMD_PROCESS_EXTRA;
}else{
return CommandProcessResultAPI::CMD_PROCESS_ERROR;
}
};
return cmd_exec;
};
EXECUTE_API(cmd_func)

// 5. Register the command with the controller
REGISTER_COMMAND_API
}

After these steps, a new motion command is created and PMoveL can be called from RL.

For more command usage, see examples/motion_cmd.cpp.