xcore_api Introduction
This page lists the controller plugin APIs available for secondary development, organized by header under the SDK xcore_api/ directory.
The current header version is 0.0.3 (macro XCORE_API_VERSION in #include "version.hpp"). The interface package README.md states that it is based on controller v3.2.1. Ensure the xcore_api version used by the plugin matches the target controller version.
launch/launch_api.hpp
| Header: | #include "launch/launch_api.hpp" |
Macros
LAUNCH_MODULE(CLASS_NAME)
LAUNCH_MODULE registers the entry class with the controller. The default priority is 0.
CLASS_NAME is the entry class name. It must derive from LaunchAPI.
- The macro takes effect when the dynamic library is loaded. Internally it calls
LaunchAPI::Register(). - If this macro or
LAUNCH_MODULE_PRIORITY()is not used, the controller does not run the lifecycle functions of that entry class.
See also LAUNCH_MODULE_PRIORITY(), LaunchAPI, Controller Plugin Entry.
LAUNCH_MODULE_PRIORITY(CLASS_NAME, priority)
Registers the entry class with the given priority. A higher priority runs Init(), Start(), and Stop() earlier. The order among the same priority is not fixed.
See also LAUNCH_MODULE(), LaunchAPI::Register().
LaunchAPI Class
The LaunchAPI class is the abstract base class of all controller plugin entry modules.
| Header: | #include "launch/launch_api.hpp" |
| Namespace: | xcore_api::launch |
Public Functions
[pure virtual] void | Init() |
[pure virtual] void | Start() |
[pure virtual] void | Stop() |
[static] bool | Register(int priority, std::shared_ptr<LaunchAPI> ptr) |
Detailed Description
The LaunchAPI class is the controller plugin entry. A derived class must implement Init(), Start(), and Stop(), and register with LAUNCH_MODULE() or LAUNCH_MODULE_PRIORITY().
The controller calls them in this order: construct, Init() by priority, Start() by priority after every Init finishes, Stop() by priority on stop, then destroy. Construction and destruction order is not fixed. Release dependent resources in Stop().
#include "launch/launch_api.hpp"
class ExamplePlugin : public xcore_api::launch::LaunchAPI {
public:
void Init() override {
// Load configuration and initialize logs
}
void Start() override {
// Register commands, services, Hooks, and log codes
}
void Stop() override {
// Release resources, stop threads, and close the bus
}
};
LAUNCH_MODULE(ExamplePlugin)
See also LAUNCH_MODULE(), Controller Plugin Entry.
Member Function Documentation
[pure virtual] void LaunchAPI::Init()
Initializes the plugin.
All entry modules run in priority order. Use this to load configuration, initialize logs, and prepare data structures.
See also Start(), InitLogAPI().
[pure virtual] void LaunchAPI::Start()
Called after every Init() has finished.
Use this to register RL commands, services, Hooks, and log codes, or start background tasks.
See also Init(), RegPluginCmdsAPI(), RegisterHooksAPI(), RegServiceAPI().
[pure virtual] void LaunchAPI::Stop()
Called when the controller stops or unloads the plugin.
Release resources, stop threads, and close device connections here.
See also Start().
[static] bool LaunchAPI::Register(int priority, std::shared_ptr<LaunchAPI> ptr)
Registers the entry module with the controller. A higher priority runs earlier. Returns true on success.
For secondary development, use LAUNCH_MODULE(). Do not call this directly.
See also LAUNCH_MODULE(), LAUNCH_MODULE_PRIORITY().
rl_cmd/morden_rl_cmd_api.hpp
| Header: | #include "rl_cmd/morden_rl_cmd_api.hpp" |
The spelling morden in the file name matches the SDK package.
Macros
BEGIN_COMMAND_API(cmd_config)
Builds an internal ModernRLCmdAPI builder from cmd_config. Use it together with PARAMS_API(), EXECUTE_API(), and REGISTER_COMMAND_API.
See also RLCmdConfigAPI, Command Registration.
PARAMS_API(...)
Sets the parameter checker for the current command. The arguments are one or more ArgTypeAPI values.
EXECUTE_API(lambda)
Sets the forward executor. The lambda type is RLCmdActionAPI.
EXECUTE_STB_API(lambda)
Sets the step-back executor. Use this when the step-back type is STEP_BACK_CUSTOM.
REGISTER_COMMAND_API
Registers the command built so far with the controller. Internally calls RegPluginCmdsAPI().
Call this from the entry module Start().
See also RegPluginCmdsAPI().
Enum Types
enum class xcore_api::rl_cmd::ValueTypeAPI
This enum type describes command argument types. The type must match the RL call site before you read an argument.
| Constant | Description |
|---|---|
ValueTypeAPI::VALUE_UNKNOWN | Unknown type |
ValueTypeAPI::VALUE_INT | Integer |
ValueTypeAPI::VALUE_DOUBLE | Floating point |
ValueTypeAPI::VALUE_BOOL | Boolean |
ValueTypeAPI::VALUE_STRING | String |
ValueTypeAPI::VALUE_BYTE | Byte |
ValueTypeAPI::VALUE_CLOCK | Clock |
ValueTypeAPI::VALUE_CONFDATA | Configuration data |
ValueTypeAPI::VALUE_FCBOXVOL / VALUE_FCCARTNUM / VALUE_FCCYLINDERVOL / VALUE_FCSPHEREVOL / VALUE_FCXYZNUM | Force-control related |
ValueTypeAPI::VALUE_INTNUM | Integer array |
ValueTypeAPI::VALUE_JOINTTARGET | Joint target |
ValueTypeAPI::VALUE_LOAD | Load |
ValueTypeAPI::VALUE_ORIENT | Orientation |
ValueTypeAPI::VALUE_PATH | Path |
ValueTypeAPI::VALUE_POS | Position |
ValueTypeAPI::VALUE_POSE | Pose |
ValueTypeAPI::VALUE_ROBTARGET | Cartesian point |
ValueTypeAPI::VALUE_SPEED | Speed |
ValueTypeAPI::VALUE_TOOL | Tool |
ValueTypeAPI::VALUE_TRIGDATA | Trigger |
ValueTypeAPI::VALUE_WOBJ | Work object |
ValueTypeAPI::VALUE_ZONE | Zone |
ValueTypeAPI::VALUE_SIGNAL_DI / VALUE_SIGNAL_DO / VALUE_SIGNAL_GI / VALUE_SIGNAL_GO / VALUE_SIGNAL_AI / VALUE_SIGNAL_AO | IO signal |
ValueTypeAPI::VALUE_MODBUS | Modbus |
ValueTypeAPI::VALUE_INPUT_SIGNAL | Input signal |
ValueTypeAPI::VALUE_TRANS | Extra switch parameter, for example \Stop |
ValueTypeAPI::VALUE_KEY_PARA | Keyword parameter |
ValueTypeAPI::VALUE_SWITCH | On / Off |
ValueTypeAPI::VALUE_TORQUE_INFO / VALUE_JOINT_TORQUE / VALUE_CART_TORQUE | Torque information |
ValueTypeAPI::VALUE_SOCKET_SERVER / VALUE_SOCKET_CONNECT | Network control |
ValueTypeAPI::VALUE_NULL | Null type |
See also ArgTypeAPI, SymbolVarBaseAPI.
enum class xcore_api::rl_cmd::ArgRuleTypeAPI
This enum type describes default-argument rules.
| Constant | Value | Description |
|---|---|---|
ArgRuleTypeAPI::ARG_MUST_HAVE | 0 | Required |
ArgRuleTypeAPI::ARG_DEFAULT_AT_LAST | 1 | Optional at the end of the argument list |
ArgRuleTypeAPI::ARG_DEFAULT_NOT_LAST | 2 | Optional, not at the end of the argument list |
enum xcore_api::rl_cmd::CommandProcessResultAPI
This enum type describes the command result returned by the inner executor.
| Constant | Value | Description |
|---|---|---|
CMD_PROCESS_SUCCESS | 0 | Success. RL continues |
CMD_PROCESS_ERROR | 1 | Failure. Only the current task pauses |
CMD_PROCESS_FATAL | 2 | Fatal error. RL stops |
CMD_PROCESS_IGNORE | 3 | Async command. The task enters async wait |
CMD_PROCESS_EXTRA | 4 | Extra executed command, often used for motion |
CMD_PROCESS_RESCHEDULE | 5 | Request reschedule |
CMD_PROCESS_SPECIAL | 6 | Special command. Affects scheduling |
See also RLCmdActionAPI, SendCmd().
enum xcore_api::rl_cmd::CmdLookAheadImplAPI
This enum type describes command look-ahead behavior.
| Constant | Value | Description |
|---|---|---|
WAIT_MOVE_PAUSE | 0 | Wait for motion to finish and break look-ahead (default) |
ACTIVATE_AT_LOOKAHEAD | 1 | Trigger at look-ahead, for example print-style commands |
ACTIVATE_IN_ZONE | 2 | Trigger in the zone, after the previous motion |
MOVEMENT_ITSELF | 3 | The motion command itself |
Commands that involve motion must set look-ahead correctly so they do not break controller scheduling.
See also RLCmdConfigAPI::SetLookAhead(), Custom Motion Commands.
enum xcore_api::rl_cmd::TaskLimitAPI
This enum type describes the task limit of a command.
| Constant | Value | Description |
|---|---|---|
TASK_NO_LIMIT | 0 | No limit |
TASK_LIMIT_MOVE | 1 | Limit motion tasks |
TASK_LIMIT_NORMAL_AND_STATIC | 2 | Limit normal and semi-static tasks |
enum xcore_api::rl_cmd::StepBackAPI
This enum type describes step-back behavior.
| Constant | Value | Description |
|---|---|---|
STEP_BACK_SKIP | 0 | Skip this command |
STEP_BACK_STOP | 1 | Stop step-back |
STEP_BACK_CUSTOM | 2 | Custom behavior with EXECUTE_STB_API() |
Types
using xcore_api::rl_cmd::CommandExecuteAPI = std::function<CommandProcessResultAPI()>
Inner command executor. Returns CommandProcessResultAPI.
using xcore_api::rl_cmd::RLCmdActionAPI
Outer command factory. The signature is:
std::function<CommandExecuteAPI(
std::shared_ptr<RLCallFrameAPI>,
std::vector<std::shared_ptr<SymbolVarBaseAPI>>)>
The outer factory builds the inner CommandExecuteAPI at schedule time. The inner function runs the command logic.
See also RLCallFrameAPI, SymbolVarBaseAPI.
ArgTypeAPI Class
The ArgTypeAPI class describes the type, default rule, and default value of one command argument.
| Header: | #include "rl_cmd/morden_rl_cmd_api.hpp" |
| Namespace: | xcore_api::rl_cmd |
Public Functions
ArgTypeAPI() | |
ArgTypeAPI(ValueTypeAPI type) | |
ArgTypeAPI(std::vector<ValueTypeAPI> types) | |
ArgTypeAPI(ValueTypeAPI type, ArgRuleTypeAPI arg_rule, SymbolVarBaseAPI value) | |
ArgTypeAPI(std::vector<ValueTypeAPI> types, ArgRuleTypeAPI arg_rule, SymbolVarBaseAPI value) | |
void | SetValueType(const ValueTypeAPI &type) |
void | SetRule(const ArgRuleTypeAPI &rule) |
void | SetDefaultValue(const SymbolVarBaseAPI &value) |
std::vector<ValueTypeAPI> | GetValueType() const |
ArgRuleTypeAPI | GetRule() const |
std::shared_ptr<SymbolVarBaseAPI> | GetDefaultValue() const |
Detailed Description
Required arguments are constructed with a single type or a type list. Optional arguments must also provide ArgRuleTypeAPI and a default value.
See also PARAMS_API(), ValueTypeAPI.
Member Function Documentation
void ArgTypeAPI::SetValueType(const ValueTypeAPI &type)
Sets the argument type.
void ArgTypeAPI::SetRule(const ArgRuleTypeAPI &rule)
Sets the default-argument rule.
void ArgTypeAPI::SetDefaultValue(const SymbolVarBaseAPI &value)
Sets the default value used when the argument is omitted.
std::vector<ValueTypeAPI> ArgTypeAPI::GetValueType() const
Returns the list of types this argument accepts.
ArgRuleTypeAPI ArgTypeAPI::GetRule() const
Returns the default-argument rule.
std::shared_ptr<SymbolVarBaseAPI> ArgTypeAPI::GetDefaultValue() const
Returns the default value.
RLCmdConfigAPI Class
The RLCmdConfigAPI class describes the name, look-ahead, task limit, and step-back behavior of one custom RL command.
| Header: | #include "rl_cmd/morden_rl_cmd_api.hpp" |
| Namespace: | xcore_api::rl_cmd |
Public Functions
RLCmdConfigAPI() | |
RLCmdConfigAPI(std::shared_ptr<RLCmdConfigImpl> ptr) | |
void | SetFuncName(const std::string &func_name) |
void | SetLookAhead(const CmdLookAheadImplAPI &look_ahead) |
void | SetTaskLimit(const TaskLimitAPI &limit) |
void | SetStepBack(const StepBackAPI &step_type) |
std::string | GetFuncName() const |
CmdLookAheadImplAPI | GetLookAhead() const |
TaskLimitAPI | GetTaskLimit() const |
StepBackAPI | GetStepBack() const |
Detailed Description
Fill in the configuration before BEGIN_COMMAND_API(). The default look-ahead is WAIT_MOVE_PAUSE. Motion commands must set look-ahead to MOVEMENT_ITSELF.
See also Command Registration, Custom Motion Commands.
Member Function Documentation
void RLCmdConfigAPI::SetFuncName(const std::string &func_name)
Sets the command function name. It must match the name used in RL.
void RLCmdConfigAPI::SetLookAhead(const CmdLookAheadImplAPI &look_ahead)
Sets the look-ahead mode. The default breaks look-ahead.
See also CmdLookAheadImplAPI.
void RLCmdConfigAPI::SetTaskLimit(const TaskLimitAPI &limit)
Sets the task limit.
void RLCmdConfigAPI::SetStepBack(const StepBackAPI &step_type)
Sets the step-back type.
std::string RLCmdConfigAPI::GetFuncName() const
Returns the command function name.
CmdLookAheadImplAPI RLCmdConfigAPI::GetLookAhead() const
Returns the look-ahead type.
TaskLimitAPI RLCmdConfigAPI::GetTaskLimit() const
Returns the task limit.
StepBackAPI RLCmdConfigAPI::GetStepBack() const
Returns the step-back behavior.
RLCallFrameAPI Class
The RLCallFrameAPI class provides the runtime context of the current command and can set a return value.
| Header: | #include "rl_cmd/morden_rl_cmd_api.hpp" |
| Namespace: | xcore_api::rl_cmd |
Public Functions
RLCallFrameAPI(std::shared_ptr<RLCallFrameImpl> ptr) | |
std::string | GetCmdTask() |
std::string | GetCmdFile() |
int | GetCmdLine() |
int | GetVisitedLine() |
void | SetReturnValue(const SymbolVarBaseAPI &val) |
Member Function Documentation
std::string RLCallFrameAPI::GetCmdTask()
Returns the current task name.
std::string RLCallFrameAPI::GetCmdFile()
Returns the current file name.
int RLCallFrameAPI::GetCmdLine()
Returns the current line number.
int RLCallFrameAPI::GetVisitedLine()
Returns the visited line number.
void RLCallFrameAPI::SetReturnValue(const SymbolVarBaseAPI &val)
Sets the command return value.
See also SymbolVarBaseAPI.
ModernRLCmdAPI Class
The ModernRLCmdAPI class is the custom-command builder. Secondary development usually uses the macros and does not instantiate this class directly.
| Header: | #include "rl_cmd/morden_rl_cmd_api.hpp" |
| Namespace: | xcore_api::rl_cmd |
Public Functions
| explicit | ModernRLCmdAPI(const RLCmdConfigAPI &cfg) |
| virtual | ~ModernRLCmdAPI() |
RLCmdConfigAPI | GetCmdConfig() |
const std::vector<std::shared_ptr<SymbolVarBaseAPI>> & | GetCmdArgs() |
void | SetParams(const std::initializer_list<ArgTypeAPI> &v) |
void | SetExecutor(RLCmdActionAPI &action) |
void | SetExecutorStb(RLCmdActionAPI &action) |
ModernRLCmdAPI | Convert() |
Detailed Description
The BEGIN_COMMAND_API() macro constructs this object. PARAMS_API(), EXECUTE_API(), EXECUTE_STB_API(), and REGISTER_COMMAND_API call SetParams(), SetExecutor(), SetExecutorStb(), and RegPluginCmdsAPI() respectively.
Do not block for a long time in a command executor. Use the thread pool for long-running work.
See also Command Registration.
Member Function Documentation
RLCmdConfigAPI ModernRLCmdAPI::GetCmdConfig()
Returns the current command configuration.
const std::vector<std::shared_ptr<SymbolVarBaseAPI>> &ModernRLCmdAPI::GetCmdArgs()
Returns the current command argument symbol table.
void ModernRLCmdAPI::SetParams(const std::initializer_list<ArgTypeAPI> &v)
Sets the parameter checker. Use PARAMS_API().
void ModernRLCmdAPI::SetExecutor(RLCmdActionAPI &action)
Sets the forward executor. Use EXECUTE_API().
void ModernRLCmdAPI::SetExecutorStb(RLCmdActionAPI &action)
Sets the step-back executor. Use EXECUTE_STB_API().
ModernRLCmdAPI ModernRLCmdAPI::Convert()
Converts this object into a registerable command. Called by REGISTER_COMMAND_API.
SymbolVarBaseAPI Class
The SymbolVarBaseAPI class reads and writes the concrete value of a command argument.
| Header: | #include "rl_cmd/morden_rl_cmd_api.hpp" |
| Namespace: | xcore_api::rl_cmd |
Public Functions
SymbolVarBaseAPI() | |
SymbolVarBaseAPI(std::shared_ptr<SymbolVarBaseImpl> ptr) | |
SymbolVarBaseAPI | GetSubUnit(const std::string &key) |
double | GetDoubleVal() |
bool | GetBoolVal() |
int | GetIntVal() |
unsigned char | GetByteVal() |
std::string | GetStringVal() |
PointAPI | GetPointAPI() |
SpeedAPI | GetSpeedAPI() |
ZoneAPI | GetZoneAPI() |
ToolAPI | GetToolAPI() |
WobjAPI | GetWobjAPI() |
void | ResetRobTarget(const PointAPI &point) |
void | ResetBool(bool val) |
void | ResetInt(int val) |
void | ResetDouble(double val) |
void | ResetString(const std::string &val) |
void | ResetBoolArr(const std::vector<bool> &v) |
void | ResetIntArr(const std::vector<int> &v) |
void | ResetDoubleArr(const std::vector<double> &v) |
void | ResetStringArr(const std::vector<std::string> &v) |
Detailed Description
Confirm the argument type before reading. For composite values (for example a quaternion inside a Cartesian point), enter the child field with GetSubUnit(). When the type does not match, the basic readers return 0 / false / an empty string.
See also ValueTypeAPI, PointAPI.
Member Function Documentation
SymbolVarBaseAPI SymbolVarBaseAPI::GetSubUnit(const std::string &key)
Reads a child unit of a composite value by key.
double SymbolVarBaseAPI::GetDoubleVal()
Returns a double. Returns 0 when the type does not match.
bool SymbolVarBaseAPI::GetBoolVal()
Returns a bool.
int SymbolVarBaseAPI::GetIntVal()
Returns an int.
unsigned char SymbolVarBaseAPI::GetByteVal()
Returns the byte value.
std::string SymbolVarBaseAPI::GetStringVal()
Returns the string.
PointAPI SymbolVarBaseAPI::GetPointAPI()
Returns the point.
See also PointAPI.
SpeedAPI SymbolVarBaseAPI::GetSpeedAPI()
Returns the speed.
ZoneAPI SymbolVarBaseAPI::GetZoneAPI()
Returns the zone.
ToolAPI SymbolVarBaseAPI::GetToolAPI()
Returns the tool.
WobjAPI SymbolVarBaseAPI::GetWobjAPI()
Returns the work object.
void SymbolVarBaseAPI::ResetRobTarget(const PointAPI &point)
Writes the robtarget argument as point.
void SymbolVarBaseAPI::ResetBool(bool val)
Writes the Boolean argument as val.
void SymbolVarBaseAPI::ResetInt(int val)
Writes the integer argument as val.
void SymbolVarBaseAPI::ResetDouble(double val)
Writes the floating-point argument as val.
void SymbolVarBaseAPI::ResetString(const std::string &val)
Writes the string argument as val.
void SymbolVarBaseAPI::ResetBoolArr(const std::vector<bool> &v)
Overwrites the Boolean array. The length must match.
void SymbolVarBaseAPI::ResetIntArr(const std::vector<int> &v)
Overwrites the integer array.
void SymbolVarBaseAPI::ResetDoubleArr(const std::vector<double> &v)
Overwrites the floating-point array.
void SymbolVarBaseAPI::ResetStringArr(const std::vector<std::string> &v)
Overwrites the string array.
Related Non-Members
std::shared_ptr<RLCmdArgImpl> xcore_api::rl_cmd::RequireArgsAPI(const std::vector<ArgTypeAPI> &v)
Builds a command-argument object from a type list. Secondary development usually uses PARAMS_API() and does not call this directly.
bool xcore_api::rl_cmd::RegPluginCmdsAPI(std::shared_ptr<ModernRLCmdAPI> ptr)
Registers the command with the controller. Returns true on success. For secondary development, use REGISTER_COMMAND_API.
See also REGISTER_COMMAND_API.
motion_cmd/motion_cmd_api.hpp
| Header: | #include "motion_cmd/motion_cmd_api.hpp" |
Usually used with a custom RL command: parse arguments into MotionCmdArgsAPI, then enqueue them with MotionCmdAPI.
Enum Types
enum xcore_api::motion_cmd::MoveTypeAPI
This enum type describes the motion type.
| Constant | Value | Description |
|---|---|---|
MOVE_ABSJ | 0 | Absolute joint motion |
MOVE_J | 1 | Joint motion |
MOVE_L | 2 | Linear motion |
MOVE_C | 3 | Circular motion |
MOVE_CF | 4 | Full-circle motion. Call SetMoveCFData() |
MOVE_T | 5 | Trochoid motion. Call SetMoveTData() |
MOVE_SP | 6 | Spiral motion. Call SetMoveSPData() |
enum xcore_api::motion_cmd::RotTypeAPI
This enum type describes the orientation rotation mode of a full-circle motion.
| Constant | Description |
|---|---|
CONST_POSE | Keep orientation |
ROT_AXIS | Rotating-axis rotation |
FIXED_AXIS | Fixed-axis rotation |
enum xcore_api::motion_cmd::CallBackTypeAPI
This enum type describes the motion callback type.
| Constant | Value | Description |
|---|---|---|
MOVE_START | 0 | Motion start |
MOVE_PAUSE | 1 | Motion pause |
MOVE_FINISH | 2 | Motion finish |
MOVE_ERROR | 3 | Motion error |
See also MotionCmdArgsAPI::SetCallback().
MotionCmdArgsAPI Class
The MotionCmdArgsAPI class describes the target, type, tool, work object, speed, zone, triggers, and callbacks of one motion command.
| Header: | #include "motion_cmd/motion_cmd_api.hpp" |
| Namespace: | xcore_api::motion_cmd |
Public Functions
Detailed Description
Pose, speed, and distance use SI units: position in meters, angles usually in radians. Unless noted otherwise, members return 0 on success.
Do not block for a long time in a callback or Trigger.
See also MotionCmdAPI, Custom Motion Commands, PointAPI.
Member Function Documentation
int MotionCmdArgsAPI::SetTargetPoint(const PointAPI &point)
Sets the target point. Returns 0 on success.
int MotionCmdArgsAPI::SetMoveType(const MoveTypeAPI &type)
Sets the motion type.
See also MoveTypeAPI.
int MotionCmdArgsAPI::SetMoveCFData(RotTypeAPI type, double rundeg)
Sets extra parameters for a full circle. Use this with MOVE_CF. rundeg is the execution angle, from -359 to 3600 degrees.
int MotionCmdArgsAPI::SetMoveTData(double radius, double step)
Sets extra parameters for a trochoid. Use this with MOVE_T. radius and step are in meters.
int MotionCmdArgsAPI::SetMoveSPData(double radius, double step, double angle, bool clockwise)
Sets extra parameters for a spiral. Use this with MOVE_SP. radius is in meters, step is in m/rad, and angle is in radians. clockwise is true for clockwise.
int MotionCmdArgsAPI::SetTool(const ToolAPI &tool)
Sets the tool.
int MotionCmdArgsAPI::SetWobj(const WobjAPI &wobj)
Sets the work object.
int MotionCmdArgsAPI::SetZone(const ZoneAPI &zone)
Sets the zone.
int MotionCmdArgsAPI::SetSpeed(const SpeedAPI &speed)
Sets the speed.
int MotionCmdArgsAPI::SetLast(bool last)
Marks this command as the last of a continuous motion. When last is true, the current continuous motion ends.
int MotionCmdArgsAPI::SetUpdatePointer(const std::string &task_name, const std::string &file_name, int line)
Updates the client execution pointer. The task, file, and line can be taken from RLCallFrameAPI.
int MotionCmdArgsAPI::SetCallback(CallBackTypeAPI type, const std::function &func)
Sets the callback for motion start, pause, finish, or error.
See also CallBackTypeAPI.
int MotionCmdArgsAPI::SetAuxPoint(const PointAPI &point)
Sets the auxiliary point. Multi-point motions such as arcs use this.
int MotionCmdArgsAPI::SetTriggers(const std::vector<TriggerAPI> &triggers)
Sets path triggers. MOVE_ABSJ does not support this.
See also TriggerAPI.
int MotionCmdArgsAPI::SetFinishInAdvance(double distance = 0.002)
Finishes this path early. Combine this with a Trigger or IO for search-style commands. distance is the maximum stop distance in meters. The default is 2 mm.
MotionCmdAPI Class
The MotionCmdAPI class sends motion parameters to the controller motion queue.
| Header: | #include "motion_cmd/motion_cmd_api.hpp" |
| Namespace: | xcore_api::motion_cmd |
Public Functions
MotionCmdAPI() | |
| virtual | ~MotionCmdAPI() |
int | SendCmd(const MotionCmdArgsAPI &args) |
int | SendSegmentCmds(const std::vector<MotionCmdArgsAPI> &vargs) |
int | SendStepBackCmd(const MotionCmdArgsAPI &args) |
Detailed Description
Confirm the controller mode, task space, and robot busy state before sending. Returns 0 on success. The RL result of a motion command is usually CMD_PROCESS_EXTRA.
Warning: This changes the robot motion state.
See also StatesAPI, Custom Motion Commands.
Member Function Documentation
int MotionCmdAPI::SendCmd(const MotionCmdArgsAPI &args)
Sends one motion command. Returns 0 on success.
See also SendSegmentCmds().
int MotionCmdAPI::SendSegmentCmds(const std::vector<MotionCmdArgsAPI> &vargs)
Sends multiple interrupted continuous motions. Each segment pauses after it finishes, then the next starts. The next segment starts only after the previous one has finished.
Use this when one RL command contains multiple path segments.
See also SendCmd().
int MotionCmdAPI::SendStepBackCmd(const MotionCmdArgsAPI &args)
Builds and sends a step-back command.
sdk/sdk_cmd_api.hpp
| Header: | #include "sdk/sdk_cmd_api.hpp" |
Enum Types
enum class xcore_api::sdk_cmd::Status
This enum type describes the execution status of a non-motion SDK command.
| Constant | Description |
|---|---|
Status::SUCCESS | Command finished |
Status::PENDING | Running |
Status::ERROR | Execution error. The command reports it itself |
SDKCmdAPI Class
The SDKCmdAPI class is the base class of non-motion commands that can enter the SDK command queue.
| Header: | #include "sdk/sdk_cmd_api.hpp" |
| Namespace: | xcore_api::sdk_cmd |
Public Functions
SDKCmdAPI() | |
| virtual | ~SDKCmdAPI() |
[virtual] void | BeforeProcess() |
[pure virtual] Status | DerivedProcess() |
[virtual] void | AfterProcess() |
Detailed Description
A derived class must implement DerivedProcess(). It may override the before and after callbacks. Enqueue the command with MordenSDKCmdAPI::SendSDKCmd().
Member Function Documentation
[virtual] void SDKCmdAPI::BeforeProcess()
Callback before the command runs. The default implementation is empty.
[pure virtual] Status SDKCmdAPI::DerivedProcess()
Core command logic. Returns Status.
[virtual] void SDKCmdAPI::AfterProcess()
Callback after the command runs. The default implementation is empty.
MordenSDKCmdAPI Class
The MordenSDKCmdAPI class sends motion or non-motion commands into the SDK command queue. The spelling Morden in the class name matches the header.
| Header: | #include "sdk/sdk_cmd_api.hpp" |
| Namespace: | xcore_api::sdk_cmd |
Public Functions
MordenSDKCmdAPI() | |
| virtual | ~MordenSDKCmdAPI() |
int | SendSDKMotionCmd(const MotionCmdArgsAPI &args, int cmd_id) |
int | SendSDKCmd(std::shared_ptr<SDKCmdAPI> ptr, int cmd_id) |
void | SetFinalSDKCmd() |
Member Function Documentation
int MordenSDKCmdAPI::SendSDKMotionCmd(const MotionCmdArgsAPI &args, int cmd_id)
Sends one SDK motion command. cmd_id is the command identifier. Returns 0 on success.
See also MotionCmdArgsAPI.
int MordenSDKCmdAPI::SendSDKCmd(std::shared_ptr<SDKCmdAPI> ptr, int cmd_id)
Sends one ordinary SDK command. Returns 0 on success.
See also SDKCmdAPI.
void MordenSDKCmdAPI::SetFinalSDKCmd()
Sets the command that breaks look-ahead.
hooks/
Corresponds to #include "hooks/hooks_api.hpp" and #include "hooks/hooks_args_api.hpp". After a plugin registers a Hook, the controller calls it when the matching event occurs. See hooks Module.
| Header: | #include "hooks/hooks_api.hpp", #include "hooks/hooks_args_api.hpp" |
Enum Types
enum xcore_api::hooks::HookEventAPI
This enum type describes the controller events that can be registered.
| Constant | Description |
|---|---|
INVALID_EVENT | Invalid event |
POINT_CHANGE | Point create, delete, or modify |
PP_TO_MAIN | Program pointer jumps to the main program |
PP_TO_LINE | Program pointer jumps to a given line |
B_START_RUN | Start running |
B_PAUSE_RUN | Pause running |
E_STOP_RUN | Emergency stop |
enum xcore_api::hooks::RunTypeAPI
This enum type describes how a Hook callback runs.
| Constant | Description |
|---|---|
SYNC_RUN | Synchronous. Blocks the matching controller event |
ASYNC_RUN_IN_THREAD_POOL | Asynchronous in the ordinary thread pool |
ASYNC_RUN_IN_RT_THREAD | Runs on a real-time thread |
Do not do long-running work in a synchronous Hook.
enum xcore_api::hooks::CURDAPI
This enum type describes a point-change operation.
| Constant | Description |
|---|---|
CREATE | Create |
UPDATE | Update |
READ | Read |
DELETE | Delete |
Types
using xcore_api::hooks::FUNC = std::function<void(const std::shared_ptr<const HookArgsBaseAPI>)>
Hook callback type. For events with arguments, dynamically cast the argument to the matching derived type, for example HookPPToLineArgsAPI.
HookDataAPI Class
The HookDataAPI class describes the event, callback, run type, and priority to register.
| Header: | #include "hooks/hooks_api.hpp" |
| Namespace: | xcore_api::hooks |
Public Functions
HookDataAPI() | |
| virtual | ~HookDataAPI() |
bool | SetEvent(HookEventAPI event) |
bool | SetHook(const FUNC &hook) |
bool | SetRunType(RunTypeAPI type) |
bool | SetPriority(int pri) |
const HookEventAPI | GetEvent() const |
const FUNC | GetHook() const |
const RunTypeAPI | GetRunType() const |
const int | GetPriority() const |
Detailed Description
Registration flow: construct HookDataAPI, call SetEvent() and SetHook(), optionally SetRunType() and SetPriority(), then call RegisterHooksAPI().
RegisterHooksAPI()does not accept dynamic registration after pluginStart().UnRegisterHooksAPI()takes effect only after every plugin has finished Start.
See also RegisterHooksAPI(), hooks Module.
Member Function Documentation
bool HookDataAPI::SetEvent(HookEventAPI event)
Sets the event type. Returns true on success.
bool HookDataAPI::SetHook(const FUNC &hook)
Sets the callback. Returns true on success.
bool HookDataAPI::SetRunType(RunTypeAPI type)
Sets synchronous or asynchronous execution. Returns true on success.
bool HookDataAPI::SetPriority(int pri)
Sets the schedule priority. A higher value is scheduled earlier. Returns true on success.
const HookEventAPI HookDataAPI::GetEvent() const
Returns the configured event.
const FUNC HookDataAPI::GetHook() const
Returns the callback.
const RunTypeAPI HookDataAPI::GetRunType() const
Returns the run type.
const int HookDataAPI::GetPriority() const
Returns the priority.
HookArgsBaseAPI Class
The HookArgsBaseAPI class is the base class of all Hook arguments.
| Header: | #include "hooks/hooks_args_api.hpp" |
| Namespace: | xcore_api::hooks |
It has no business members. Events with arguments are cast in the callback to HookPointArgsAPI or HookPPToLineArgsAPI.
HookPointArgsAPI Class
The HookPointArgsAPI class describes the point name and create/update/delete operation of POINT_CHANGE.
| Header: | #include "hooks/hooks_args_api.hpp" |
| Inherits: | HookArgsBaseAPI |
Public Functions
HookPointArgsAPI() | |
const std::string | GetPointName() const |
bool | SetPointName(const std::string &name) |
const CURDAPI | GetOperate() const |
bool | SetOperate(const CURDAPI &operate) |
Member Function Documentation
const std::string HookPointArgsAPI::GetPointName() const
Returns the point name.
bool HookPointArgsAPI::SetPointName(const std::string &name)
Sets the point name. Returns true on success.
const CURDAPI HookPointArgsAPI::GetOperate() const
Returns the create / delete / update operation.
bool HookPointArgsAPI::SetOperate(const CURDAPI &operate)
Sets the operation type. Returns true on success.
HookPPToLineArgsAPI Class
The HookPPToLineArgsAPI class describes the task, file, and line of PP_TO_LINE.
| Header: | #include "hooks/hooks_args_api.hpp" |
| Inherits: | HookArgsBaseAPI |
Public Functions
HookPPToLineArgsAPI() | |
const std::string | GetFileName() const |
bool | SetFileName(const std::string &name) |
const int | GetFileLine() const |
bool | SetFileLine(const int line) |
const std::string | GetTaskName() const |
bool | SetTaskName(const std::string &name) |
Member Function Documentation
const std::string HookPPToLineArgsAPI::GetFileName() const
Returns the jump-target file name.
bool HookPPToLineArgsAPI::SetFileName(const std::string &name)
Sets the file name. Returns true on success.
const int HookPPToLineArgsAPI::GetFileLine() const
Returns the jump-target line.
bool HookPPToLineArgsAPI::SetFileLine(const int line)
Sets the line number. Returns true on success.
const std::string HookPPToLineArgsAPI::GetTaskName() const
Returns the task name.
bool HookPPToLineArgsAPI::SetTaskName(const std::string &name)
Sets the task name. Returns true on success.
Related Non-Members
int xcore_api::hooks::RegisterHooksAPI(const HookDataAPI &data)
Registers the Hook with the controller. A return value greater than 0 is the hook id and means success. -1 means failure.
Does not accept dynamic registration after plugin Start().
See also UnRegisterHooksAPI(), HookDataAPI.
int xcore_api::hooks::UnRegisterHooksAPI(int hook_id)
Removes a registered Hook by hook_id. Call this only after every plugin has finished Start. Returns 0 on success.
See also RegisterHooksAPI().
states/states_api.hpp
| Header: | #include "states/states_api.hpp" |
Enum Types
enum xcore_api::states::TaskSpaceAPI
This enum type describes task-space occupancy.
| Constant | Description |
|---|---|
TS_READY | Idle |
TS_BUSY | Busy |
enum xcore_api::states::RunningStateAPI
This enum type describes the current robot invocation stage.
| Constant | Value | Description |
|---|---|---|
RS_NONE | 0 | None |
RS_START | 1 | Start |
RS_PAUSE | 2 | Pause |
RS_STEP | 3 | Step |
RS_BACK | 4 | Step back |
RS_ERROR_HANDLER | 5 | Error handling |
RS_RESET | 6 | Reset |
RS_COLLISION | 7 | Collision |
RS_STOP_EVENT | 8 | Emergency stop |
RS_NUM_NEVER_USE | 9 | Sentinel. Do not use |
StatesAPI Class
The StatesAPI class queries or sets controller runtime state.
| Header: | #include "states/states_api.hpp" |
| Namespace: | xcore_api::states |
Public Functions
StatesAPI() | |
| virtual | ~StatesAPI() |
bool | IsAutoMode() |
bool | SetAutoMode(bool mode) |
bool | IsPowerOn() |
bool | SetPowerOn(bool on) |
bool | IsTaskSpaceReady() |
int | SetTaskSpace(const TaskSpaceAPI &space, bool busy) |
bool | IsRobotBusy() |
bool | SetRobotBusy(bool busy) |
RunningStateAPI | GetRunningState() |
bool | IsSimuMode() |
Detailed Description
Confirm the current mode and task state before changing controller state. When combining this with motion or task control, first check whether the action is allowed.
SetRobotBusy() and SetTaskSpace() must occupy and release in pairs. Otherwise other modules may be blocked from using the robot.
See also RLTaskAPI, MotionCmdAPI.
Member Function Documentation
bool StatesAPI::IsAutoMode()
Returns whether the controller is in auto mode. true is auto, false is manual.
See also SetAutoMode().
bool StatesAPI::SetAutoMode(bool mode)
Sets auto / manual mode. mode true selects auto. Returns true on success.
Warning: This changes the controller operating mode.
See also IsAutoMode().
bool StatesAPI::IsPowerOn()
Returns whether the controller is powered on.
See also SetPowerOn().
bool StatesAPI::SetPowerOn(bool on)
Sets power on / off. on true powers on. Returns true on success.
Warning: This changes the controller power state.
See also IsPowerOn().
bool StatesAPI::IsTaskSpaceReady()
Returns whether the task space is idle and available.
See also SetTaskSpace().
int StatesAPI::SetTaskSpace(const TaskSpaceAPI &space, bool busy)
Sets task-space occupancy. Occupies when space is TS_BUSY and busy is true. Releases and returns to Ready when busy is false. Returns 0 on success.
See also IsTaskSpaceReady(), TaskSpaceAPI.
bool StatesAPI::IsRobotBusy()
Returns whether the robot is occupied. true means busy and unavailable.
See also SetRobotBusy().
bool StatesAPI::SetRobotBusy(bool busy)
Sets the robot busy / idle. Use this in pairs. Returns true on success.
See also IsRobotBusy().
RunningStateAPI StatesAPI::GetRunningState()
Returns the current running stage.
See also RunningStateAPI.
bool StatesAPI::IsSimuMode()
Returns whether the controller is in simulation. true is simulation, false is a real robot.
rl_task/rl_task_api.hpp
| Header: | #include "rl_task/rl_task_api.hpp" |
RLTaskAPI Class
The RLTaskAPI class controls and queries RL program tasks.
| Header: | #include "rl_task/rl_task_api.hpp" |
| Namespace: | xcore_api::rl_task |
Public Functions
Detailed Description
If a jump fails, the interpreter state may become uncontrolled. Reload the task if needed. Pointer line numbers may be off by 1.
Warning: StopRun() deletes the task. After stop, reload the task before running again.
Member Function Documentation
bool RLTaskAPI::PPToMain()
Resets the program pointer to the main program. Returns true on success.
See also IsProgramResetDone().
bool RLTaskAPI::IsProgramResetDone()
Returns whether program reset has finished.
bool RLTaskAPI::PPToLine(const int line, const std::string &task_name = "", const std::string &file_name = "")
Jumps to the given task, file, and line. When both task_name and file_name are empty, single-task mode jumps to line in the currently executing file.
If the jump fails, the state is uncontrolled. Reload the task.
See also PPToFunc(), PPToMain().
bool RLTaskAPI::PPToFunc(const int line, const std::string &task_name = "", const std::string &file_name = "")
Jumps to the given function, mainly for debugging. When the last two arguments are empty, single-task mode jumps to a function in the currently executing file.
If the jump fails, the interpreter state is uncontrolled. Reload the task.
bool RLTaskAPI::ModifyProgramLoop(bool prog_loop)
Changes the loop mode. prog_loop true runs in a loop.
bool RLTaskAPI::AlarmRLTask(const std::string &name)
Wakes the task named name. Returns true on success.
bool RLTaskAPI::StartRun()
Starts program execution. Returns true on success.
See also PauseRun(), StopRun().
bool RLTaskAPI::PauseRun()
Pauses RL. It can be started again later. Returns true on success.
See also StartRun(), PauseRunAndWaitIdle().
bool RLTaskAPI::PauseRunAndWaitIdle(int timeout_ms = 2000)
Pauses the program and waits for the robot to stop. timeout_ms defaults to 2000 and is usually no more than 500 ms.
bool RLTaskAPI::PauseTask(const std::string &task_name)
Pauses only the specified task.
bool RLTaskAPI::StopRun()
Stops execution. Stopping deletes the task. Reload it before running again.
Warning: This changes the controller task state.
See also StartRun().
std::pair<std::string, int> RLTaskAPI::GetPointedLine(const std::string &task_name = "")
Returns the file and line of the program pointer. The line may be off by 1.
See also SetPointedLine(), GetExecLine().
std::pair<std::string, int> RLTaskAPI::GetExecLine(const std::string &task_name = "")
Returns the file and line of the motion pointer. The line may be off by 1.
See also SetExecLine().
int RLTaskAPI::SetPointedLine(const std::string &task_name, const std::string &file_name, int line)
Sets the program pointer. Returns 0 on success.
int RLTaskAPI::SetExecLine(const std::string &task_name, const std::string &file_name, int line)
Sets the motion pointer. Returns 0 on success.
bool RLTaskAPI::IsTaskExists(const std::string &name)
Returns whether a task named name exists.
bool RLTaskAPI::IsTaskRunning(const std::string &task_name)
bool RLTaskAPI::IsTaskRunning()
The overload with task_name checks whether that task is running. The no-argument overload checks whether any task is running.
These are overloaded functions.
io/analog_api.hpp
| Header: | #include "io/analog_api.hpp" |
Analog Class
The Analog class provides access to AI / AO / DI / DO / GI / GO and internal registers.
| Header: | #include "io/analog_api.hpp" |
| Access: | Analog::getInstance() |
| Namespace: | xcore_api::io |
Public Functions
Detailed Description
Get the singleton with getInstance(). Signal read/write returns true on success and false if the signal does not exist. Register read/write returns 0 on success. AI / DI / GI are read-only.
Confirm that the name, address, data type, and target architecture match before reading or writing.
Warning: Writing AO / DO / GO or a register changes field signals.
See also Communication Module.
Member Function Documentation
[static] Analog *Analog::getInstance()
Returns the Analog singleton.
bool Analog::GetAIValue(const std::string &signal_name, double &value)
Reads AI. Writes value on success. Returns false if the signal does not exist.
bool Analog::GetAOValue(const std::string &signal_name, double &value)
Reads AO.
See also SetAOValue().
bool Analog::SetAOValue(const std::string &signal_name, const double value)
Writes AO.
Warning: This changes field analog output.
bool Analog::GetDIValue(const std::string &signal_name, bool &value)
Reads DI.
bool Analog::GetDOValue(const std::string &signal_name, bool &value)
Reads DO.
See also SetDOValue().
bool Analog::SetDOValue(const std::string &signal_name, const bool value)
Writes DO.
Warning: This changes field digital output.
bool Analog::GetGIValue(const std::string &signal_name, unsigned int &value)
Reads GI.
bool Analog::GetGOValue(const std::string &signal_name, unsigned int &value)
Reads GO.
See also SetGOValue().
bool Analog::SetGOValue(const std::string &signal_name, const unsigned int value)
Writes GO. Returns false if the signal does not exist or the value is out of range.
int Analog::WriteInt16Register(const std::string &name, const int16_t &value, int bias)
Writes an int16 register by name and offset. Returns 0 on success.
See also ReadInt16Register().
int Analog::WriteBoolRegister(const std::string &name, const bool &value, int bias)
Writes a bool register.
int Analog::WriteFloatRegister(const std::string &name, const float &value, int bias)
Writes a float register.
int Analog::WriteBitRegister(const std::string &name, const bool &value, int bias)
Writes a bit register.
int Analog::WriteInt32Register(const std::string &name, const int32_t &value, int bias)
Writes an int32 register.
int Analog::WriteByteRegister(const std::string &name, const uint8_t &value, int bias)
Writes a byte register.
int Analog::ReadInt16Register(const std::string &name, int16_t &value, int bias)
Reads an int16 register.
int Analog::ReadBoolRegister(const std::string &name, bool &value, int bias)
Reads a bool register.
int Analog::ReadFloatRegister(const std::string &name, float &value, int bias)
Reads a float register.
int Analog::ReadBitRegister(const std::string &name, bool &value, int bias)
Reads a bit register.
int Analog::ReadInt32Register(const std::string &name, int32_t &value, int bias)
Reads an int32 register.
int Analog::ReadByteRegister(const std::string &name, uint8_t &value, int bias)
Reads a byte register.
bool Analog::IsAiExist(const std::string &signal_name)
Returns whether the AI exists.
bool Analog::IsAoExist(const std::string &signal_name)
Returns whether the AO exists.
bool Analog::IsDiExist(const std::string &signal_name)
Returns whether the DI exists.
bool Analog::IsDoExist(const std::string &signal_name)
Returns whether the DO exists.
bool Analog::IsGiExist(const std::string &signal_name)
Returns whether the GI exists.
bool Analog::IsGoExist(const std::string &signal_name)
Returns whether the GO exists.
bool Analog::RegisterType(const std::string ®ister_name, std::string &type)
Looks up the register type by name and writes type (int16, bool, float, bit, int32, byte). Returns false if the register does not exist.
bool Analog::RegisterWriteable(const std::string ®ister_name, bool &writeable)
Queries whether the register is writable. Returns false if the register does not exist.
bool Analog::CheckRegisterCanUsedAsIO(const std::string ®ister_name, const std::string &io_type)
Returns whether the register can stand in for the given IO type. Returns true when it can.
registers/function_code_api.hpp
| Header: | #include "registers/function_code_api.hpp" |
A plugin can declare a function-code class, define supported register types, length, and read/write attributes, and implement the execution logic. After registration it appears in the HMI function-code list. See Communication Module.
Macros
DECLARE_FUNCTION_CODE_API(type_name)
Declares function-code class type_name, makes it inherit FuncCodeAPI, and implements Clone().
See also FUNCTION_CODE_EXECUTE_API(), RegFuncCodeAPI().
FUNCTION_CODE_EXECUTE_API(type_name)
Defines the ExecFuncCode() body of type_name.
Enum Types
enum xcore_api::registers::RegTypeAPI
This enum type describes the register data type.
| Constant | Description |
|---|---|
BIT | Bit |
BOOL | Boolean |
BYTE | Byte |
INT16 | 16-bit integer |
INT32 | 32-bit integer |
FLOAT | Floating point |
FuncCodeCfgAPI Class
The FuncCodeCfgAPI class describes the function-code name, supported types, length, and whether it is writable.
| Header: | #include "registers/function_code_api.hpp" |
| Namespace: | xcore_api::registers |
Public Functions
FuncCodeCfgAPI() | |
| virtual | ~FuncCodeCfgAPI() |
bool | SetName(const std::string &name) |
std::string | GetName() |
bool | SetSupportType(const std::vector<RegTypeAPI> &v) |
std::vector<RegTypeAPI> | GetSupportType() |
bool | SetLen(uint32_t len) |
uint32_t | GetLen() |
bool | SetWriteable(bool writeable) |
bool | IsWriteable() |
Member Function Documentation
bool FuncCodeCfgAPI::SetName(const std::string &name)
Sets the function-code name. Returns true on success.
std::string FuncCodeCfgAPI::GetName()
Returns the function-code name.
bool FuncCodeCfgAPI::SetSupportType(const std::vector<RegTypeAPI> &v)
Sets the set of supported register types.
std::vector<RegTypeAPI> FuncCodeCfgAPI::GetSupportType()
Returns the set of supported types.
bool FuncCodeCfgAPI::SetLen(uint32_t len)
Sets the register length.
uint32_t FuncCodeCfgAPI::GetLen()
Returns the register length.
bool FuncCodeCfgAPI::SetWriteable(bool writeable)
Sets the read/write attribute. writeable true is a write type, false is a read type.
A read-only register runs the function code when the value changes. A write-only register writes the register after the function code runs.
bool FuncCodeCfgAPI::IsWriteable()
Returns whether this is a write type.
FuncCodeAPI Class
The FuncCodeAPI class is the function-code base class. A derived class must implement ExecFuncCode() and Clone().
| Header: | #include "registers/function_code_api.hpp" |
| Namespace: | xcore_api::registers |
Public Functions
FuncCodeAPI(const FuncCodeCfgAPI &cfg) | |
| virtual | ~FuncCodeAPI() |
[pure virtual] bool | ExecFuncCode() |
[pure virtual] std::shared_ptr<FuncCodeAPI> | Clone() |
FuncCodeCfgAPI | GetCfg() |
int | ReadIntRegValue(std::vector<int> &v) |
int | ReadFloatRegValue(std::vector<float> &v) |
int | WriteIntRegValue(const std::vector<int> &v) |
int | WriteFloatRegValue(const std::vector<float> &v) |
Detailed Description
Declare a derived class with DECLARE_FUNCTION_CODE_API(), then register it with RegFuncCodeAPI().
See also Communication Module.
Member Function Documentation
[pure virtual] bool FuncCodeAPI::ExecFuncCode()
Function-code execution logic. Returns true on success.
[pure virtual] std::shared_ptr<FuncCodeAPI> FuncCodeAPI::Clone()
Clones the current function-code instance. DECLARE_FUNCTION_CODE_API() already provides a default implementation.
FuncCodeCfgAPI FuncCodeAPI::GetCfg()
Returns the function-code configuration.
int FuncCodeAPI::ReadIntRegValue(std::vector<int> &v)
Reads the associated integer registers. Returns 0 on success.
int FuncCodeAPI::ReadFloatRegValue(std::vector<float> &v)
Reads the associated floating-point registers. Returns 0 on success.
int FuncCodeAPI::WriteIntRegValue(const std::vector<int> &v)
Writes integer registers. Returns 0 on success.
int FuncCodeAPI::WriteFloatRegValue(const std::vector<float> &v)
Writes floating-point registers. Returns 0 on success.
Related Non-Members
bool xcore_api::registers::RegFuncCodeAPI(std::shared_ptr<FuncCodeAPI> ptr)
Registers the function code with the controller. Returns true on success. Call this from Init().
See also DECLARE_FUNCTION_CODE_API().
ethercat/ecat_base_api.hpp
| Header: | #include "ethercat/ecat_base_api.hpp" |
See const_data/ecat_api.hpp for PDO / SDO data structures. See Communication Module for usage.
EcatBaseAPI Class
The EcatBaseAPI class operates PDO and SDO of a given slave. Secondary development usually inherits this class, registers objects in the derived class, then reads and writes.
| Header: | #include "ethercat/ecat_base_api.hpp" |
| Namespace: | xcore_api::ecat |
Public Functions
EcatBaseAPI(uint16_t slave_id) | |
| virtual | ~EcatBaseAPI() |
int | GetPdoValue(const PdoAPI &obj, void *value, bool bOutputData = false) |
int | SetPdoValue(const PdoAPI &obj, void *value) |
int | SetSdoValue(SdoAPI &sdo, void *value) |
int | GetSdoValue(SdoAPI &sdo, void *value) |
Protected Functions
Detailed Description
Pass the slave ID to the constructor. The data pointer must be large enough for the object. Unless noted otherwise, 0 means success.
Member Function Documentation
int EcatBaseAPI::GetPdoValue(const PdoAPI &obj, void *value, bool bOutputData = false)
Reads PDO. bOutputData true reads output data, false reads input data. The buffer pointed to by value must be large enough. Returns 0 on success.
See also SetPdoValue(), PdoAPI.
int EcatBaseAPI::SetPdoValue(const PdoAPI &obj, void *value)
Writes PDO. Returns 0 on success.
int EcatBaseAPI::SetSdoValue(SdoAPI &sdo, void *value)
Writes SDO. Returns 0 on success.
See also GetSdoValue(), SdoAPI.
int EcatBaseAPI::GetSdoValue(SdoAPI &sdo, void *value)
Reads SDO. Returns 0 on success.
bool EcatBaseAPI::InitEcat()
Initializes EtherCAT. Returns true on success. Call this from a derived-class initialization flow.
int EcatBaseAPI::RegisterPdo(PdoAPI &pdo, uint16_t baseIndex, uint16_t byteoffs, uint16_t byteLen)
Registers a PDO with the given base index, byte offset, and length. Returns 0 on success.
int EcatBaseAPI::RegisterSdo(SdoAPI &sdo, uint16_t index, uint16_t subIndex, uint16_t dateLen, uint16_t timeOut, const ThreadFunc &func)
Registers an SDO. The spellings dateLen and timeOut match the header. Returns 0 on success.
fieldbus/fieldbus_api.hpp
| Header: | #include "fieldbus/fieldbus_api.hpp" |
Wraps creating, configuring, opening, and closing fieldbus devices, plus register read/write and DI / DO access. See Communication Module.
Enum Types
enum xcore_api::fieldbus::DeviceTypeAPI
This enum type describes the fieldbus device type.
| Constant | Description |
|---|---|
MODBUS_TCP_MASTER | Modbus TCP master |
MODBUS_TCP_SLAVER | Modbus TCP slave |
MODBUS_RTU_MASTER | Modbus RTU master |
MODBUS_RTU_SLAVER | Modbus RTU slave |
PROFINET_SLAVER | Profinet slave |
EIP_SLAVER | EtherNet/IP slave |
CCLINK_IE_SLAVER | CC-Link IE slave |
CCLINK_ECAT_SLAVER | CC-Link EtherCAT slave |
The spelling SLAVER in the constant names matches the header.
enum xcore_api::fieldbus::EndianAPI
This enum type describes the endianness of register data.
| Constant | Description |
|---|---|
ABCD | Big endian |
CDAB | Big-endian bytes, little-endian words |
BADC | Little-endian bytes, big-endian words |
DCBA | Little-endian bytes and words |
FieldbusCfgAPI Class
The FieldbusCfgAPI class is the base configuration of a fieldbus device, including device type, name, and endianness.
| Header: | #include "fieldbus/fieldbus_api.hpp" |
| Namespace: | xcore_api::fieldbus |
Public Functions
FieldbusCfgAPI() | |
FieldbusCfgAPI(DeviceTypeAPI type) | |
| virtual | ~FieldbusCfgAPI() |
void | Reset(DeviceTypeAPI type) |
int | SetName(const std::string &value) |
std::string | GetName() |
int | SetEndian(EndianAPI endian) |
EndianAPI | GetEndian() |
Member Function Documentation
void FieldbusCfgAPI::Reset(DeviceTypeAPI type)
Resets the device type.
int FieldbusCfgAPI::SetName(const std::string &value)
Sets the device name. Returns 0 on success.
std::string FieldbusCfgAPI::GetName()
Returns the device name. The default is empty.
int FieldbusCfgAPI::SetEndian(EndianAPI endian)
Sets the endianness. Returns 0 on success.
EndianAPI FieldbusCfgAPI::GetEndian()
Returns the endianness.
ModbusCfgAPI Class
The ModbusCfgAPI class describes the IP, port, serial port, slave ID, and register / coil counts of Modbus TCP / RTU.
| Header: | #include "fieldbus/fieldbus_api.hpp" |
| Inherits: | FieldbusCfgAPI |
Public Functions
ModbusCfgAPI(DeviceTypeAPI type) | |
void | SetIp(const std::string &value) |
const std::string | GetIp() const |
void | SetPort(const uint32_t &value) |
const uint32_t | GetPort() const |
void | SetSerialName(const std::string &value) |
const std::string | GetSerialName() const |
void | SetSlaverId(const uint32_t &value) |
const uint32_t | GetSlaverId() const |
void | SetHoldRegStartAddr(const uint32_t &value) |
const uint32_t | GetHoldRegStartAddr() const |
void | SetHoldRegNum(const uint32_t &value) |
const uint32_t | GetHoldRegNum() const |
void | SetInputRegStartAddr(const uint32_t &value) |
const uint32_t | GetInputRegStartAddr() const |
void | SetInputRegNum(const uint32_t &value) |
const uint32_t | GetInputRegNum() const |
void | SetCoilsStartAddr(const uint32_t &value) |
const uint32_t | GetCoilsStartAddr() const |
void | SetCoilsNum(const uint32_t &value) |
const uint32_t | GetCoilsNum() const |
void | SetDiscInputStartAddr(const uint32_t &value) |
const uint32_t | GetDiscInputStartAddr() const |
void | SetDiscInputNum(const uint32_t &value) |
const uint32_t | GetDiscInputNum() const |
Detailed Description
TCP types use SetIp() and SetPort(). RTU types use SetSerialName(). If a slave does not support reading coils or discrete inputs, set the corresponding count to 0. Otherwise function may be affected.
Member Function Documentation
void ModbusCfgAPI::SetIp(const std::string &value)
Sets the IP. Valid only for Modbus TCP.
const std::string ModbusCfgAPI::GetIp() const
Returns the IP.
void ModbusCfgAPI::SetPort(const uint32_t &value)
Sets the port. Valid only for Modbus TCP.
const uint32_t ModbusCfgAPI::GetPort() const
Returns the port.
void ModbusCfgAPI::SetSerialName(const std::string &value)
Sets the serial-port name. Valid only for Modbus RTU.
const std::string ModbusCfgAPI::GetSerialName() const
Returns the serial-port name.
void ModbusCfgAPI::SetSlaverId(const uint32_t &value)
Sets the slave ID. The spelling Slaver in the function name matches the header.
const uint32_t ModbusCfgAPI::GetSlaverId() const
Returns the slave ID.
void ModbusCfgAPI::SetHoldRegStartAddr(const uint32_t &value)
Sets the holding-register start address.
const uint32_t ModbusCfgAPI::GetHoldRegStartAddr() const
Returns the holding-register start address.
void ModbusCfgAPI::SetHoldRegNum(const uint32_t &value)
Sets the holding-register count.
const uint32_t ModbusCfgAPI::GetHoldRegNum() const
Returns the holding-register count.
void ModbusCfgAPI::SetInputRegStartAddr(const uint32_t &value)
Sets the input-register start address.
const uint32_t ModbusCfgAPI::GetInputRegStartAddr() const
Returns the input-register start address.
void ModbusCfgAPI::SetInputRegNum(const uint32_t &value)
Sets the input-register count.
const uint32_t ModbusCfgAPI::GetInputRegNum() const
Returns the input-register count.
void ModbusCfgAPI::SetCoilsStartAddr(const uint32_t &value)
Sets the coil start address.
const uint32_t ModbusCfgAPI::GetCoilsStartAddr() const
Returns the coil start address.
void ModbusCfgAPI::SetCoilsNum(const uint32_t &value)
Sets the coil count. Set this to 0 if the slave does not support it.
const uint32_t ModbusCfgAPI::GetCoilsNum() const
Returns the coil count.
void ModbusCfgAPI::SetDiscInputStartAddr(const uint32_t &value)
Sets the discrete-input start address.
const uint32_t ModbusCfgAPI::GetDiscInputStartAddr() const
Returns the discrete-input start address.
void ModbusCfgAPI::SetDiscInputNum(const uint32_t &value)
Sets the discrete-input count. Set this to 0 if the slave does not support it.
const uint32_t ModbusCfgAPI::GetDiscInputNum() const
Returns the discrete-input count.
ProfinetCfgAPI Class
The ProfinetCfgAPI class describes the Profinet station name, NIC, update period, and slot module IDs.
| Header: | #include "fieldbus/fieldbus_api.hpp" |
| Inherits: | FieldbusCfgAPI |
Public Functions
ProfinetCfgAPI(DeviceTypeAPI type) | |
void | SetStationName(const std::string &value) |
const std::string | GetStationName() const |
void | SetNetcard(const std::string &value) |
const std::string | GetNetcard() const |
void | SetUpdateDataInternal(const uint32_t &value) |
const uint32_t | GetUpdateDataInternal() const |
void | SetSlot1ModuleID(const uint32_t &value) |
const uint32_t | GetSlot1ModuleID() const |
void | SetSlot2ModuleID(const uint32_t &value) |
const uint32_t | GetSlot2ModuleID() const |
void | SetSlot3MmoduleID(const uint32_t &value) |
const uint32_t | GetSlot3ModuleID() const |
void | SetSlot4ModuleID(const uint32_t &value) |
const uint32_t | GetSlot4ModuleID() const |
void | SetSlot5ModuleID(const uint32_t &value) |
const uint32_t | GetSlot5ModuleID() const |
void | SetSlot6ModuleID(const uint32_t &value) |
const uint32_t | GetSlot6ModuleID() const |
Member Function Documentation
void ProfinetCfgAPI::SetStationName(const std::string &value)
Sets the station name.
const std::string ProfinetCfgAPI::GetStationName() const
Returns the station name.
void ProfinetCfgAPI::SetNetcard(const std::string &value)
Sets the NIC. The spelling Netcard in the function name matches the header.
const std::string ProfinetCfgAPI::GetNetcard() const
Returns the NIC.
void ProfinetCfgAPI::SetUpdateDataInternal(const uint32_t &value)
Sets the update period. The spelling Internal in the function name matches the header.
const uint32_t ProfinetCfgAPI::GetUpdateDataInternal() const
Returns the update period.
void ProfinetCfgAPI::SetSlot1ModuleID(const uint32_t &value)
Sets the slot 1 module ID. The setters for slots 2, 4, 5, and 6 work the same way.
const uint32_t ProfinetCfgAPI::GetSlot1ModuleID() const
Returns the slot 1 module ID. The getters for slots 2 through 6 work the same way.
void ProfinetCfgAPI::SetSlot2ModuleID(const uint32_t &value)
Sets the slot 2 module ID.
const uint32_t ProfinetCfgAPI::GetSlot2ModuleID() const
Returns the slot 2 module ID.
void ProfinetCfgAPI::SetSlot3MmoduleID(const uint32_t &value)
Sets the slot 3 module ID. The spelling Mmodule in the function name matches the header.
const uint32_t ProfinetCfgAPI::GetSlot3ModuleID() const
Returns the slot 3 module ID.
void ProfinetCfgAPI::SetSlot4ModuleID(const uint32_t &value)
Sets the slot 4 module ID.
const uint32_t ProfinetCfgAPI::GetSlot4ModuleID() const
Returns the slot 4 module ID.
void ProfinetCfgAPI::SetSlot5ModuleID(const uint32_t &value)
Sets the slot 5 module ID.
const uint32_t ProfinetCfgAPI::GetSlot5ModuleID() const
Returns the slot 5 module ID.
void ProfinetCfgAPI::SetSlot6ModuleID(const uint32_t &value)
Sets the slot 6 module ID.
const uint32_t ProfinetCfgAPI::GetSlot6ModuleID() const
Returns the slot 6 module ID.
EipCfgAPI Class
The EipCfgAPI class describes the EtherNet/IP read/write register counts and NIC.
| Header: | #include "fieldbus/fieldbus_api.hpp" |
| Inherits: | FieldbusCfgAPI |
Public Functions
EipCfgAPI(DeviceTypeAPI type) | |
void | SetReadRegNum(const uint16_t &value) |
const uint16_t | GetReadRegNum() const |
void | SetWriteRegNum(const uint16_t &value) |
const uint16_t | GetWriteRegNum() const |
void | SetNetCard(const std::string &value) |
const std::string | GetNetCard() const |
Member Function Documentation
void EipCfgAPI::SetReadRegNum(const uint16_t &value)
Sets the read-register count.
const uint16_t EipCfgAPI::GetReadRegNum() const
Returns the read-register count.
void EipCfgAPI::SetWriteRegNum(const uint16_t &value)
Sets the write-register count.
const uint16_t EipCfgAPI::GetWriteRegNum() const
Returns the write-register count.
void EipCfgAPI::SetNetCard(const std::string &value)
Sets the NIC.
const std::string EipCfgAPI::GetNetCard() const
Returns the NIC.
CCLinkCfgAPI Class
The CCLinkCfgAPI class describes the CC-Link protocol type, NIC, occupied station count, baud rate, and protocol version.
| Header: | #include "fieldbus/fieldbus_api.hpp" |
| Inherits: | FieldbusCfgAPI |
Public Functions
CCLinkCfgAPI(DeviceTypeAPI type) | |
void | SetProtoType(const std::string &value) |
const std::string | GetProtoType() const |
void | SetNetCard(const std::string &value) |
const std::string | GetNetCard() const |
void | SetOccupiedStaNum(const uint32_t &value) |
const uint32_t | GetOccupiedStationNum() const |
void | SetBaudRate(const uint32_t &value) |
const uint32_t | GetBaudRate() const |
void | SetProtoVersion(const uint32_t &value) |
const uint32_t | GetProtoVersion() const |
Member Function Documentation
void CCLinkCfgAPI::SetProtoType(const std::string &value)
Sets the protocol type.
const std::string CCLinkCfgAPI::GetProtoType() const
Returns the protocol type.
void CCLinkCfgAPI::SetNetCard(const std::string &value)
Sets the NIC.
const std::string CCLinkCfgAPI::GetNetCard() const
Returns the NIC.
void CCLinkCfgAPI::SetOccupiedStaNum(const uint32_t &value)
Sets the occupied station count.
const uint32_t CCLinkCfgAPI::GetOccupiedStationNum() const
Returns the occupied station count.
void CCLinkCfgAPI::SetBaudRate(const uint32_t &value)
Sets the baud rate.
const uint32_t CCLinkCfgAPI::GetBaudRate() const
Returns the baud rate.
void CCLinkCfgAPI::SetProtoVersion(const uint32_t &value)
Sets the protocol version.
const uint32_t CCLinkCfgAPI::GetProtoVersion() const
Returns the protocol version.
FieldbusAPI Class
The FieldbusAPI class provides a unified API to open, close, read/write registers, and access DI / DO.
| Header: | #include "fieldbus/fieldbus_api.hpp" |
| Namespace: | xcore_api::fieldbus |
Public Functions
FieldbusAPI(const FieldbusCfgAPI &cfg) | |
| virtual | ~FieldbusAPI() |
int | Open() |
int | Close() |
int | ReadRegisters(uint32_t addr, uint16_t *dest, const uint32_t &nb = 1) |
int | WriteRegisters(uint32_t addr, const uint16_t *src, const uint32_t &nb = 1) |
int | GetDINum() |
int | GetDONum() |
int | SetDO(const uint32_t &index, const bool &value) |
int | GetDI(const uint32_t &index, bool &value) |
Detailed Description
Pass FieldbusCfgAPI or a derived configuration to the constructor. Unless noted otherwise, 0 means success.
See also Communication Module.
Member Function Documentation
int FieldbusAPI::Open()
Opens the fieldbus device. Returns 0 on success.
See also Close().
int FieldbusAPI::Close()
Closes the fieldbus device. Returns 0 on success.
int FieldbusAPI::ReadRegisters(uint32_t addr, uint16_t *dest, const uint32_t &nb = 1)
Reads nb registers from addr into dest. nb defaults to 1. Returns 0 on success.
See also WriteRegisters().
int FieldbusAPI::WriteRegisters(uint32_t addr, const uint16_t *src, const uint32_t &nb = 1)
Writes nb registers from src to addr. Returns 0 on success.
int FieldbusAPI::GetDINum()
Returns the DI count.
int FieldbusAPI::GetDONum()
Returns the DO count.
int FieldbusAPI::SetDO(const uint32_t &index, const bool &value)
Sets a DO by index. Returns 0 on success.
Warning: This changes field digital output.
int FieldbusAPI::GetDI(const uint32_t &index, bool &value)
Reads a DI by index. Writes value on success.
endtool/endtool_api.hpp
| Header: | #include "endtool/endtool_api.hpp" |
Used to control devices such as electric grippers through end-tool protocol passthrough. Currently it mainly wraps Modbus RTU.
ModbusRTUEndtoolAPI Class
The ModbusRTUEndtoolAPI class wraps common Modbus RTU function codes for end tools.
| Header: | #include "endtool/endtool_api.hpp" |
| Namespace: | xcore_api::endtool |
Public Functions
Detailed Description
Use this to wrap private protocols of end tools such as grippers, tool changers, and sensors. crc_inverse controls whether CRC is inverted. Returns true on success.
Member Function Documentation
bool ModbusRTUEndtoolAPI::RWData(const int &send_len, const std::vector<uint8_t> &send_data, const int &rev_len, std::vector<uint8_t> &rev_data, int &ret_status)
Sends and receives raw data directly. ret_status is the return status.
bool ModbusRTUEndtoolAPI::ReadCoil_01(const int &slave_id, const uint16_t &addr, const int &len, std::vector<bool> &data, bool crc_inverse = false)
Reads coils. Function code 01.
bool ModbusRTUEndtoolAPI::ReadDiscreteInput_02(const int &slave_id, const uint16_t &addr, const int &len, std::vector<bool> &data, bool crc_inverse = false)
Reads discrete inputs. Function code 02.
bool ModbusRTUEndtoolAPI::ReadRegister_03(const int &slave_id, const uint16_t &addr, const uint16_t &len, std::vector<uint16_t> &data, bool crc_inverse = false)
Reads holding registers. Function code 03.
bool ModbusRTUEndtoolAPI::ReadRegister_04(const int &slave_id, const uint16_t &addr, const uint16_t &len, std::vector<uint16_t> &data, bool crc_inverse = false)
Reads input registers. Function code 04.
bool ModbusRTUEndtoolAPI::WriteCoil_05(const int &slave_id, const uint16_t &addr, const int &len, std::vector<bool> &data, bool crc_inverse = false)
Writes a single coil. Function code 05.
bool ModbusRTUEndtoolAPI::WriteRegister_06(const int &slave_id, const uint16_t &addr, const uint16_t &len, const std::vector<uint16_t> &data, bool crc_inverse = false)
Writes a single register. Function code 06.
bool ModbusRTUEndtoolAPI::WriteCoil_0F(const int &slave_id, const uint16_t &addr, const int &len, std::vector<bool> &data, bool crc_inverse = false)
Writes multiple coils. Function code 15.
bool ModbusRTUEndtoolAPI::WriteRegister_10(const int &slave_id, const uint16_t &addr, const uint16_t &len, const std::vector<uint16_t> &data, bool crc_inverse = false)
Writes multiple registers. Function code 16.
service/service_api.hpp
| Header: | #include "service/service_api.hpp" |
Registers a custom JSON protocol in a controller plugin. After the client sends a request with plugin_name and key, the controller calls the registered callback and returns the JSON it produces. See Client Interaction.
Related Non-Members
int xcore_api::service::RegServiceAPI(const std::string &plugin_name, const std::string &key, const std::function &func)
Registers one service protocol. plugin_name is the plugin name, key is the protocol key, and func receives the request JSON and returns the response JSON. Returns 0 on success.
Register this in Start(). Use it to read state, send configuration, or implement lightweight inter-plugin communication with JSON.
See also Client Interaction.
log/log_api.hpp
| Header: | #include "log/log_api.hpp" |
Initializes a plugin-specific log and provides log macros prefixed with the plugin name. See log Library Usage.
Macros
| Macro | Level |
|---|---|
LOG_DEBUG / LOG_INFO / LOG_WARNING / LOG_ERROR / LOG_FATAL | Debug / Info / Warning / Error / Fatal |
Macro Notes
The usage is similar to stream output:
LOG_INFO << "hello world";
Use the customized macros in this header. Without them, logs are written together with the controller logs. Total log storage must not exceed 1 GB.
See also InitLogAPI(), log Library Usage.
Related Non-Members
int xcore_api::log::InitLogAPI(const std::string &dir, size_t max_size, size_t max_nubmer)
Initializes plugin logs. dir is the storage directory relative to the plugin data directory. max_size is the per-file size limit in MB. max_nubmer is the file count; the parameter spelling matches the header. Returns 0 on success.
Call this from Init().
The header also declares xcore_api::log::PLUGIN, whose value is the return of GetPluginNameAPI(), for the log-level prefix.
user_log/user_log_api.hpp
| Header: | #include "user_log/user_log_api.hpp" |
Registers and reports multilingual user logs and runtime logs with the controller. Load the configuration in Init() and register log codes in Start(). See User Log Reporting.
Related Non-Members
int xcore_api::user_log::ConfigReportLogAPI(const Json::Value &val)
Configures multilingual logs for this plugin. Must be called from Init(). Returns 0 on success.
See also ConfigEnglishReportLogAPI(), RegisterReportLogAPI().
int xcore_api::user_log::ConfigEnglishReportLogAPI(const Json::Value &val)
Configures the English fallback logs. Must be called from Init(). Returns 0 on success.
int xcore_api::user_log::RegisterReportLogAPI()
Registers the configured log codes with the controller so they take effect. Must be called from Start(). Returns 0 on success.
void xcore_api::user_log::ReportUserLogAPI(int log_no, const std::string &detail = "", const std::string &context = "")
Reports a multilingual user log. log_no is the log number, detail is the detailed-reason key, and context replaces $arg in the text.
void xcore_api::user_log::ReportRunLogAPI(int log_no, const std::string &arg = "", const std::string &detail = "")
Reports a user runtime log. log_no is the RunLog number. arg replaces $arg in content. detail is shown on the client detail page.
const_data/pose_api.hpp
| Header: | #include "const_data/pose_api.hpp" |
Defines common motion data structures for controller plugins, using SI units: meters, radians, and kilograms. These types support operator<< and can be written to logs directly.
PositionAPI Struct
The PositionAPI struct describes a position in meters.
| Member | Type | Description |
|---|---|---|
x / y / z | double | Coordinates in meters |
QuaternionAPI Struct
The QuaternionAPI struct describes an orientation quaternion. The default is (1, 0, 0, 0).
| Member | Type | Description |
|---|---|---|
q1 / q2 / q3 / q4 | double | Quaternion components |
ConfDataAPI Struct
The ConfDataAPI struct describes the robot configuration used to choose a solution to the target.
| Member | Type | Description |
|---|---|---|
cfx / cf1–cf7 | int | Configuration components |
PoseAPI Struct
The PoseAPI struct describes a pose / coordinate frame.
| Member | Type | Description |
|---|---|---|
p | PositionAPI | Position |
q | QuaternionAPI | Orientation |
Supports right-multiply operator* and Inverse().
PoseAPI PoseAPI::Inverse() const
Returns the inverse of this frame.
PointAPI Struct
The PointAPI struct describes a point. It can be a Cartesian point or a joint point.
| Member | Type | Description |
|---|---|---|
pose | PoseAPI | Cartesian pose |
joint | std::vector<double> | Joint angles in radians |
is_joint | bool | Whether this is a joint point |
extjoint | std::vector<double> | External axes in radians |
is_ext_rad | bool | Header comment says “external axes are degrees”; default false |
arm_angle | double | Arm angle of a 7-axis robot |
confdata | ConfDataAPI | Configuration |
ZoneAPI Struct
The ZoneAPI struct describes a zone.
| Member | Type | Description |
|---|---|---|
distance | double | Distance in meters |
percent | double | Percent |
SpeedAPI Struct
The SpeedAPI struct describes speed.
| Member | Type | Description |
|---|---|---|
tcpvel | double | TCP linear speed in m/s |
orivel | double | Orientation speed in rad/s |
psivel | double | 7-axis arm angular speed |
percent | double | Joint-speed percent |
forced | bool | true ignores the speed slider |
LoadAPI Struct
The LoadAPI struct describes a load.
| Member | Type | Description |
|---|---|---|
mass | double | Mass in kilograms |
cog | PoseAPI | Center of gravity |
ix / iy / iz | double | Moments of inertia |
TriggerAPI Struct
The TriggerAPI struct describes a path trigger.
| Member | Type | Description |
|---|---|---|
type | TriggerType | DISTANCE or TIME |
reference_is_from_start | bool | Whether the reference is from the start |
value_from_reference | double | Value from the reference, in meters or seconds |
trigger_callback | std::function<void()> | Trigger callback |
See also MotionCmdArgsAPI::SetTriggers().
ToolAPI Struct
The ToolAPI struct describes the tool frame and tool load.
| Member | Type | Description |
|---|---|---|
rob_hold | bool | true is a handheld tool, false is an external tool |
tool_frame | PoseAPI | Tool frame |
tool_load | LoadAPI | Tool load |
WobjAPI Struct
The WobjAPI struct describes the work-object frame, user frame, and work-object load.
| Member | Type | Description |
|---|---|---|
rob_hold | bool | true is a handheld work object, false is an external work object |
wobj_frame | PoseAPI | Work-object frame relative to the user frame |
wobj_load | LoadAPI | Work-object load |
user_frame | PoseAPI | User frame |
uf_prog | bool | Whether the user frame moves |
uf_mec | std::string | Related mechanical unit |
uf_id | int | User-frame ID |
mech_unit | void * | Mechanical-unit data |
const_data/ecat_api.hpp
| Header: | #include "const_data/ecat_api.hpp" |
Defines EtherCAT PDO / SDO data structures for ethercat.
Types
using xcore_api::const_data::ecat::ThreadFunc = std::function
SDO callback type.
PdoAPI Struct
The PdoAPI struct describes a PDO.
| Member | Type | Description |
|---|---|---|
baseIndex | uint16_t | Data index |
byteOffs | uint16_t | Byte offset |
byteSize | uint16_t | Data size |
name | std::string | PDO name |
See also RegisterPdo(), GetPdoValue().
SdoAPI Struct
The SdoAPI struct describes an SDO. The default timeout is 4000.
| Member | Type | Description |
|---|---|---|
index | uint16_t | Index |
subIndex | uint8_t | Sub-index |
dateLen | uint32_t | Data length. The member spelling matches the header |
timeOut | uint32_t | Timeout |
flags | uint32_t | Flags |
m_msg_callback | ThreadFunc | Callback |
See also RegisterSdo(), GetSdoValue().
utils/filesystem_api.hpp
| Header: | #include "utils/filesystem_api.hpp" |
See json Library Usage for JSON usage examples.
Related Non-Members
bool xcore_api::utils::WriteBinaryToFileAPI(const std::string &filename, const std::string &content)
Writes binary content to filename. Returns true on success.
See also ReadBinaryFromFileAPI().
bool xcore_api::utils::ReadBinaryFromFileAPI(const std::string &filename, std::string &content)
Reads binary content from filename into content. Returns true on success.
bool xcore_api::utils::LoadFromFileAPI(Json::Value &root, const std::string &file_name)
Parses JSON from a file into root. Returns true on success.
See also LoadFromStringAPI(), SaveToFileAPI().
bool xcore_api::utils::LoadFromStringAPI(Json::Value &root, const std::string &json_str)
Parses JSON from a string into root. Returns true on success.
bool xcore_api::utils::SaveToFileAPI(const Json::Value &root, const std::string &file_name)
Writes JSON to a file. Returns true on success.
std::string xcore_api::utils::SaveToStringAPI(const Json::Value &root)
Serializes JSON to a string.
std::string xcore_api::utils::SaveToStringInLineAPI(const Json::Value &root)
Serializes JSON to a string as one line.
void xcore_api::utils::CreateEmptyJsonFileAPI(const std::string &file_name)
Creates an empty JSON file.
bool xcore_api::utils::IsJsonFileAPI(const std::string &file_name)
Returns whether file_name is a JSON file.
std::string xcore_api::utils::GetPluginNameAPI()
Returns the current plugin name.
utils/thread_pool_api.hpp
| Header: | #include "utils/thread_pool_api.hpp" |
Do not block for a long time in a synchronous Hook, custom-command executor, or motion callback. Use this API for long-running work.
Related Non-Members
std::future<void> xcore_api::utils::RunInThreadPoolAPI(const std::function<void()> &func)
Runs a function with no return value in the thread pool.
See also RunInThreadPoolIntAPI().
std::future<int> xcore_api::utils::RunInThreadPoolIntAPI(const std::function<int()> &func)
Runs a function that returns int in the thread pool. Get the result with future.get().
utils/singleton_api.hpp
| Header: | #include "utils/singleton_api.hpp" |
Macros
DECLARE_SINGLETON(type)
Declares a singleton friend inside the class so SingletonBaseAPI can construct type.
See also SINGLETON_INSTANCE().
SINGLETON_INSTANCE(type)
Returns the singleton pointer of type, equivalent to type::GetInstancePtr().
INIT_SINGLETON(type)
Initializes the singleton. Internally this is SINGLETON_INSTANCE().
SingletonBaseAPI Class
The SingletonBaseAPI class is the singleton base-class template.
| Header: | #include "utils/singleton_api.hpp" |
| Namespace: | xcore_api::utils |
Public Functions
SingletonBaseAPI(const SingletonBaseAPI &) = delete | |
SingletonBaseAPI & | operator=(const SingletonBaseAPI &) = delete |
[static] T & | GetInstance() |
[static] T * | GetInstancePtr() |
Detailed Description
A derived class must inherit SingletonBaseAPI<T>, use DECLARE_SINGLETON() inside the class, and make the constructor and destructor private.
class object : public xcore_api::utils::SingletonBaseAPI<object> {
DECLARE_SINGLETON(object);
private:
object() {}
~object() {}
};
Member Function Documentation
[static] T &SingletonBaseAPI::GetInstance()
Returns a reference to the singleton.
[static] T *SingletonBaseAPI::GetInstancePtr()
Returns a pointer to the singleton.
See also SINGLETON_INSTANCE().