Skip to main content

Release Notes

Version Changes​

[1.0.2.7] - 2026-08-03​

Release notes

Notes​

  • Fixed a value-passing error in point-data moveTo
  • Fixed an issue where variable APIs could not obtain values
  • Fixed defects in project APIs
  • Adjusted the feature description and style structure of xplugindemo

[1.0.2.6] - 2026-05-21​

Release notes

Notes​

  • Fixed a bug where disconnectXServiceData for xservice failed to unsubscribe
  • Fixed a crash that could occur when using the right-side expand widget API (CreateRightExpandWidget) without a configuration file set

Requirements​

Requires xCore 3.2.2 or later