Rokae+ Client Plugin
- The Rokae+ Client Plugin (referred to as client plugin / HMI plugin) runs on the human-machine interface of a PC or teach pendant. It is used to extend process UI, interaction, and instruction editing. It can work together with the Controller Plugin, or be used independently.
What It Can Do
- Embed custom UI (center area, status bar, side panel, physical buttons, full screen, etc.)
- Exchange data with controller plugins, read/write business data, and query robot status
- Register process instruction UI, handle events, and output logs
Lifecycle
| Stage | Description |
|---|---|
Initialization (init) | Initialize this plugin and mount UI; place association with other HMI modules in afterInit |
Association (afterInit) | Association with other HMI modules (for example, auxiliary-programming registration) |
Render (render) | UI or style work during startup (not continuous refresh) |
Ready (idle) | Enter the runnable state; implement as needed |
Unload (detach) | Release extra resources held by the plugin |
Version
Current version: 1.0.2.7. See Release Notes for changes.