Skip to main content

Overview

About This Manual​

Thank you for purchasing our company's robot system.

This document describes the following instructions for correct installation and use of the robot:

  • Usage of the robot secondary development interface SDK (Python).

Before installing and using this robot system, please read this manual and other related manuals carefully.

After reading, please keep it properly for easy access at any time.

Target Audience​

This manual is intended for:

  • Robot application development engineers.

Please ensure that the above personnel have the required knowledge of basic robot operation, Python programming, etc., and have received relevant training from our company.

How to Read the Product Manual​

This manual contains a separate safety chapter. Installation or maintenance operations can only be performed after reading the safety chapter.

Version History​

VersionDateDescription
v0.4.12024.08Added force control related interfaces, adapted for xCore version v2.2.2
v0.5.02024.12Added several new interfaces, fixed issues, adapted for xCore version v3.0.1
v0.7.02026.03Adapted to xCore version v3.2.1
v0.8.02026.7Added several interfaces, fixed issues, adapted for xCore v4.0.0; includes RL variables/points, EtherCAT, xPanel CAN/RS485, ArRobot, model gravity/jacobianDot, upgrade/backup, setCpuAffinity, etc.
v0.8.22026.8Added NetworkOptions, conveyor monitoring, diagnosis, getStateList, setRealtimeOptimization; fixed CAN int16/uint16 data