Skip to main content

Overview

About This Manual​

Thank you for purchasing our robot system.

This document records the following instructions for the correct installation and use of the robot:

  • Use of the SDK (C#) for robot secondary development interfaces.

Please read this manual and other related manuals carefully before installing and using the robot system.

After reading, please keep it properly for easy reference at any time.

Manual Audience​

This manual is intended for:

  • Robot application development engineers.

Please ensure that the above personnel have the necessary knowledge of basic robot operation, C# programming, etc., and have received relevant training from our company.

How to Read the Product Manual​

This manual contains a separate safety chapter, which must be read before performing installation or maintenance operations.

Version History​

Version NumberDateDescription
V0.3.42023.11First version, adapted to xCore version v2.1
V0.4.02024.04Added several interfaces, adapted to xCore version v2.2
V0.5.02024.12Added several interfaces, adapted to xCore version v3.0.1
v0.5.12025.07Added several interfaces, adapted to xCore version v3.0.1
v0.6.02025.07Added several interfaces, adapted to xCore version v3.1.1
v0.7.02026.01Added several interfaces, adapted to xCore version v3.2.0
v0.7.22026.6Added startJogWithExt and getMechUnit string overload, adapted to xCore version v3.2.2
v0.8.02026.7Added several interfaces, fixed issues, adapted to xCore v4.0.0; including RL variable/point, EtherCAT, xPanel CAN/RS485, ArRobot, model gravity/jacobianDot, upgrade/backup, etc.
v0.8.22026.8Added NetworkOptions, conveyor monitoring, and diagnosis; CANFrame.data changed to array<int>^; fixed garbled controller logs;