Skip to main content

Overview

About This Manual​

Thank you for purchasing our company's robot system.

This document describes the following instructions for correct installation and use of the robot:

  • Usage of the robot secondary development interface SDK (C++).

Before installing and using this robot system, please read this manual and other related manuals carefully.

After reading, please keep it properly for easy access at any time.

Target Audience​

This manual is intended for:

  • Robot application development engineers.

Please ensure that the above personnel have the required knowledge of basic robot operation, C++ programming, etc., and have received relevant training from our company.

How to Read the Product Manual​

This manual contains a separate safety chapter. Installation or maintenance operations can only be performed after reading the safety chapter.

Version History​

VersionDateDescription
v0.12022.6Initial version
v0.1.92022.09Rokae SDK initial version, adapted for xCore version v1.6.2
v0.2.82023.02Rokae SDK official version, adapted for xCore version v1.7
v0.3.32023.06Added new interfaces, optimized and fixed some issues, adapted for xCore version v2.0
v0.3.42023.10Added new interfaces, fixed issues, adapted for xCore version v2.1
v0.4.02024.04Added several new interfaces, fixed issues, adapted for xCore version v2.2
v0.4.12024.07Added E-stop reset and other interfaces, adapted for xCore version v2.2.2
v0.5.02024.12Added several new interfaces, fixed issues, adapted for xCore version v3.0.1
v0.5.12025.4Added several new interfaces, fixed issues, adapted for xCore version v3.0.2
v0.6.02025.7Added several new interfaces, fixed issues, adapted for xCore version v3.1.0
v0.7.02026.1Added several new interfaces, fixed issues, adapted for xCore version v3.2.0
v0.7.12026.3Added several new interfaces, fixed issues, adapted for xCore version v3.2.0
v0.7.22026.6Added several new interfaces, fixed issues, adapted for xCore version v3.2.2
v0.8.02026.7Added several new interfaces, fixed issues, adapted for xCore version v4.0.0; including RL variable/point, EtherCAT, xPanel CAN/RS485, ArRobot, model gravity/jacobianDot, etc.
v0.8.12026.7Added NetworkOptions, Diagnosis, getXService, setRealtimeOptimization, etc.
v0.8.22026.8Added conveyor monitoring; CANFrame::data changed to vector<int> to support int16/uint16/uint8