Skip to main content

15.4.12 Home command

15.4.12.1 Home — Return home

Explanation

It is used to make the robot return to the set Home through joint space motion

Definition

The command includes no input parameters

Example

Example 1

HomeSet(0, 30, 0, 60, 0, 90, 0);
Home();

Use the HomeSet command to set the Home and then the Home command to move the robot to the drag pose in the joint space.

Attention

Home pose setting must be enabled on the Robot Setup > Quick Turn interface or through the HomeSet command before the Home command can be used, otherwise, an error is reported.

15.4.12.2 HomeSet — Set home

Explanation

It is used to set the robot’s Home in the joint space

Definition

HomeSet (axis1, axis2, axis3, axis4, axis5, axis6, axis7 7 [, ext1, ext2, ext3, ext4, ext5, ext6]);

The parameter in is optional and can be omitted.

Axisx, data type: Double, to set the angle of each axis of the robot at Home

Ext, data type: Double, set the angle of each additional axis of the robot at Home, which can be left blank. When left blank, the angle of each additional axis is 0.

Example

Example 1

HomeSet(0, 30, 0, 60, 0, 90, 0); // if there is no additional axis
HomeSet(0, 0, 0, 0, 0, 0, 10, 10, 0, 0, 0, 0); // if there are additional axes
Home();

Use the HomeSet command to set the Home and then the Home command to move the robot to the drag pose in the joint space.

15.4.12.3 HomeSetAt — Get home settings

Explanation

It is used to obtain the setup data of the robot’s Home

Definition

HomeSetAt(index);

Return value, data type: double, joint angle, in °

Index, data type: int, to get the joint angle of the specified axis at Home. When the index is 0, return if HomeSet is enabled, 1 means enabled, and 0 disabled.

Example

Example 1

HomeSet (0, 30, 0, 60, 0, 90, 0);
double angle2 = HomeSetAt(2)

angle2 Get the joint angle of joint 2 at 30°.

15.4.12.4 HomeDef — Check if home is defined

Explanation

Determine if the Home is set

Definition

HomeDef()

Return value, data type: bool, true: Home already set, false: Home not set

15.4.12.5 HomeSpeed — Set return-home speed

Explanation

Set the running speed of Home command

Definition

HomeSpeed Speed

Example

Example 1

HomeSpeed(v1000);
Home();

Set the Home speed to V1000. Then the Home command moves the robot to Home at the speed of V1000.

15.4.12.6 HomeClr — Clear home

Explanation

Clear Home setting

Example

Example 1

HomeClr();

Clear Home set in the program. After clearing, the Home command cannot be executed.