Skip to main content

15.4.15 String operations

15.4.15.1 StrFind — Find substring

Explanation

It is used to find the position of a particular set of characters in the string from a specific location.

Definition

Return value, data type: int, the location of the first matching character. If the location is not found, the length of the returned string is added by 1.

StrFind (Str ChPos Set [\NotInSet]);

Str, data type: string, the string to be searched.

ChPos, data type: int, the starting position, starting from 1, if the location is off the boundary, an error is reported.

Set, data type: string, the character set to be matched.

[\NotInSet], identifier, to identify the character that cannot be matched in the character set.

Example

Example 1

VAR int found;
found = StrFind(“Robotics”, 1, “aeiou”); //2
  // Match from the first character "R", and find the second character "o" in the character set “aeiou”, return matching location 2.
found = StrFind(“Robotics”, 1, “aeiou” +NotInSet); //1
  // Match from the first character "R", and find the first character "R" is not in the character set "aeiou", return matching location 1.

15.4.15.2 StrLen — Get string length

Explanation

It is used to obtain the length of the string.

Definition

Return value, data type: int, the current string length, which is longer than or equal to 0.

StrLen (Str);

Str, data type: string, the string that requires the calculation of string length.

Example

Example 1

VAR int num;
num = StrLen(“Robotics”); //8

The length of the string "Robotics" is 8.

15.4.15.3 StrMap — Map characters into a new string

Explanation

It is used to back up a string, all characters in it are replaced according to the specified mapping relationship. The mapped characters correspond one by one according to their position, and the characters that are not mapped remain the same.

Definition

Return value, data type: string, the replaced string.

StrMap (Str, FromMap, ToMap);

Str, data type: string, the original string.

FromMap, data type: string, the index of the mapping.

ToMap, data type: string, the value of the mapping.

Example

Example 1

VAR string str;
str = StrMap(“Robotics”, “aeiou”, “AEIOU”) //RObOtIcs;

Map the string "Robotics", and "aeiou" is respectively mapped to "AEIOU".

Use restrictions: FromMap and ToMap have to match with each other and have to be of the same length.

15.4.15.4 StrMatch — Find matching substring

Explanation

It is used to search in a string, starting at the specified location, search for a particular format or a string, and return the matched location.

Definition

Return value, data type: int, the position of the first character of the matched string, and if there is no match, the string length plus one is returned.

StrMatch (Str, ChPos, Pattern);

Str, data type: string, the string to be searched.

ChPos, data type: int, the starting position, and if the location exceeds the length range of the string, an error is reported.

Pattern, data type: string, the format string to match.

Example

Example 1

VAR int found;
Found = StrMatch(“Robotics”, 1, “bo”) //3;

15.4.15.5 StrMemb — Check if character is in string

Explanation

It is used to check whether a character in a string belongs to a specified character set.

Definition

Return value, data type: bool, true indicates that the character in the string belongs to the specified character set. Otherwise, false is returned.

StrMemb (Str, ChPos, Set);

Str, data type: string, the string to be checked.

ChPos, data type: int, the position of the character to be checked; if it exceeds the range of the string, an error is reported.

Set, data type: string, the character set to be matched.

Example

Example 1

VAR bool memb;
memb = StrMemb(“Robotics”, 2, “aeiou”) //true;

The second character o is a member of the character set "aeiou" and true is returned.

15.4.15.6 StrOrder — Compare two strings

Explanation

It is used to compare two strings and return the Boolean value.

Definition

Return value, data type: bool, when str1<=str2, return true; otherwise, false.

StrOrder (Str1, Str2);

Str1, data type: string, the first string value.

Str2, data type: string, the second string value.

Example

Example 1

VAR bool le;
le = StrOrder(“FIRST”, “SECOND”); //true;
le = StrOrder(“FIRSTB”, “FIRST”); //false

15.4.15.7 StrPart — Extract substring

Explanation

It is used to truncate a part of a string to generate a new string.

Definition

Return value, data type: string, the truncated string, truncating a string from a specified location with a specified length.

StrPart (Str, ChPos, Len);

Str, data type: string, the original string of a truncated string.

ChPos, data type: int, the starting position, and if it exceeds the range of the string, an error is reported.

Len, data type: int, the length for truncating.

Example

Example 1

VAR string part;
part = StrPart(“Robotics”, 1, 5); //Robot

Truncate the string for a length of 5 bits from position 1 to get "Robot".

15.4.15.8 StrSplit — Split string

Explanation

It is used to split a string into an array of strings by specifying a separator

Definition

Return value, data type: string array, the array of strings obtained by splitting

StrSplit (Str [, separator]);

Str, data type: string, the original string to be split.

Separator, data type: string, a separator. All characters in the string are considered as a separator and can be defaulted. If no separators exist, space can be considered as the default separator.

Example

string str_arr[4] = StrSplit("test1, test2;test3+test4", "+, ;");

The string is split into four substrings (test1 test2 test3 test4).

Use restrictions:

  • An error is reported when the input string is blank.

  • If the split results do not match the length of the defined string, an error is reported.

15.4.15.9 StrToByte — String to byte

Explanation

StrToByte can convert a string into byte type data

Definition

Return value, data type: byte, the conversion result of a string.

StrToByte (Str, [ trans]));

Str, data type: string, the string to be converted.

Trans, data type: enumeration, the mathematical binary format of the string. Available parameters include \Bin (binary), \Okt (octal), \Hex (hexadecimal), \Char (character), and the default (no parameter, decimal)

Example

Example 1

Byte NumBin = StrToByte(“10”, \Bin);
Byte NumOkt = StrToByte(“10”, \Okt);
Byte NumBin = StrToByte(“10”);
Byte NumHex = StrToByte(“10”, \Hex);

The string "10" is converted to byte numbers in binary, octal, decimal, and hexadecimal in order, and the results are 2, 8, 10 and 16.

Example 2

Byte NumChar = StrToByte(“0”, \Char);

The character "0" is converted to 48 according to the conversion relationship between characters and ASCII.

Use restrictions: An error will be reported when the input string does not conform to the specified data format.

15.4.15.10 StrToDouble — String to double

Explanation

StrToDouble can convert a string into double type data

Definition

Return value, data type: double, the conversion result of a string.

StrToDouble (Str);

Str, data type: string, the string to be converted.

Example

Example 1:

Double NumDouble = StrToDouble(“3.1415926”);

Convert string "3.1415926" into double type data.

Use restrictions:

An error will be reported when the input string does not conform to the specified data format.

15.4.15.11 StrToInt — String to integer

Explanation

StrToInt can convert a string into Int type data

Definition

Return value, data type: Int, the conversion result of a string.

StrToDouble (Str);

Str, data type: string, the string to be converted.

Example

Example 1

Int NumInt = StrToInt(“99”);

Convert string "99" into Int type data.

Use restrictions: An error will be reported when the input string does not conform to the specified data format.

15.4.15.12 StrToDoubleArray — String to double array

Explanation

StrToDoubleArray can convert a large number of strings double into the type of double array data

Definition

Return value, data type: Int, to determine whether the conversion is abnormal. -1: error, 0: normal.

StrToDoubleArray(output, input, spilit);

Output, data type: double array, the output of conversion results

Input, data type: str string, the input of strings

Spilit, data type: str string, a delimiter of Double strings

Example

Example 1

string tmp_ss = "1, 2, 3, 4, 5, 6, 7";
double db_arr;
StrToDoubleArray (db_arr, tmp_ss, ", ");

Use restrictions:

The string allows for an extra terminator at the end

In case of conversion failure or including illegal characters, it will report an error, that is, "The input string is not in Double form after segmentation"

The data volume of double array should be greater than or equal to that of the data in the string; otherwise, it will report an error, that is, "The input array size is insufficient, or the array is not a one-dimensional array"