15.4.17 Clock commands
15.4.17.1 ClkRead — Read clock
Explanation |
It is used to read the value of the clock. |
Definition |
Return value, data type: double, to return the time interval between the stop time of the clock or the current time and the start of the clock. The accuracy is 0.001s. ClkRead (Clock); Clock, data type: clock, name of the clock. |
Example |
Example 1
interval stores the time interval between start and stop of clock1. |
15.4.17.2 ClkReset — Reset clock
Explanation |
It is used to reset a clock. ClkReset guarantees that the count is 0 before using a clock. |
Definition |
ClkReset (Clock); Clock, data type: clock, name of the clock. |
Example |
Example 1
Reset clock1. |
15.4.17.3 ClkStart — Start clock
Explanation |
It is used to start a clock. When a clock starts, it will continue to count until the clock stops or the program resets. The clock will continue to operate after the program stops or the robot is powered off. |
Definition |
ClkStart (Clock); Clock, data type: clock, name of the clock. |
Example |
Example 1
Declare clock1, and start clock1. |
15.4.17.4 ClkStop — Stop clock
Explanation |
It is used to stop a clock. When the clock stops, it stops counting. After the clock stops, it can be read for the interval, restarted, or reset. |
Definition |
ClkStop (Clock); Clock, data type: clock, name of the clock. |
Example |
Example 1
|