Skip to main content

变量类型

15.1 Variable Type

15.1.1 Int

Explanation

The range of the integer int variable is -2147483647−2147483647. It is recommended that the value is within the specified range. If the value is in excess of the range, it will be assigned randomly, and the maximum value range must not be exceeded when using it.

Example

In the variable list:

image727

It represents the data counter that defines an integer global variable type, and its initial value is 4.

15.1.2 Double

Explanation

Floating-point numbers, are stored using 8 bytes. Do not exceed the value range when using them.

Example

In the variable list:

image728

It represents the local variable time that defines a floating point, and its initial value is 1.5.

15.1.3 Bool

Explanation

The variable bool is mainly used for status or logic judgments. The value is true or false.

When it is assigned an int or double value, non-zero takes the value of true and zero takes the value of false.

Example

In the variable list:

image729

It indicates that a bool type global variable ifClose is defined and the initial value is true.

15.1.4 String

Explanation

String-type variables consist of multiple letters or numbers.

Note: They must be placed in double quotation marks "" at the time of defining in RL text.

Example

In the variable list:

image730

It indicates that a string variable name is defined and initialized to "rokae".

String type variables support the "+" operation for string concatenation, which can achieve string concatenation.

Example:

name = “Rok” + “ae”

It means that the variable name is assigned to "Rokae".

15.1.5 Array

Explanation

An array is a collection of variables of the same type, either one-dimensional or multi-dimensional. The elements in the array are accessed using subscripts. The subscript of each dimension begins with 1. The total length of the array should not exceed 1000.

Example

In the variable list:

image731

It indicates that a two-dimensional array that contains 16 integer variables is defined. The value of the sixth element of line 1 is assigned to 8.

15.1.6 byte

Explanation

byte represents the unsigned byte in RL language, same as unsigned char in C++.

The value range is 0−255, and negative values are not allowed. It is generally used in SocketSendByte instruction.

When the byte variable’s value exceeds 255, it is automatically truncated, keeping only the lower 8 bits of the value, e.g. var byte data2=288, and the value of data2 is 32 after truncation.

Example

In the variable list:

image732

It defines a byte variable data, which has a value of 177.

15.1.7 clock

Explanation

The clock is used for timing, and clock-related commands are just like a stopwatch used for timing.

The time accuracy of clock type storage is 0.001s, and the maximum time interval is 45 days (i.e., 45 x 24 x 3600 seconds).

Example

In the variable list:

image733

The following example shows how to use variable clock:

Example 1:

ClkStart (clock1);

ClkStop (clock1);

interval=ClkRead(clock1);

ClkReset (clock1);

Interval (pre-declared double variable) reads the interval between ClkStart and ClkStop, in seconds (s).

15.1.8 Implicit type conversion

Explanation

Currently, during data setup in the variable lists, data types are restricted. Values that do not match the variable type cannot be successfully entered, thus avoiding implicit type conversion.

Example

When defining the integer counter in the variable list, no decimals, only integers, can be entered.

15.1.9 Confdata

Explanation

The confdata (Robot Configuration Data) is used to define the morphological configuration data that corresponds to the spatial target point.

Since the robot mostly uses a rotary joint, any one of the joints exhibits the same status at 1° and 361°. Therefore, after the form of robot is selected, other measures are required to deal with the multiple-loop problem of the joint.

For example, when the joint angle is between 0° and 90°, the quadrant number is 0. When the joint angle is between 90° and 180°, it is marked as 1 and is increased/decreased by 1 for every 90°. When the angle is negative, the corresponding number of quadrants is also negative, as shown in the following figure (left: negative joint angle; right: positive joint angle). For robot joints, the angle increases when rotating anticlockwise and decreases when rotating clockwise. In the figure below, the joint angle decreases as the joint rotates clockwise, and the corresponding confdata changes as -1->-2->-3->-4 and 3->2->1->0, respectively.

For the xMate CR and SR collaborative robots, we directly record the rounded-down values of each joint angle in confdata.

In addition, the same Cartesian space target point corresponds to different inverse kinematics, so it is necessary to use confdata to specify the form to be selected.

image735

Definition

7 parameters are needed to complete the confdata, including:

cf1, data type: int, the quadrant that corresponds to the Axis 1 angle or the rounded-down joint angle.

cf2, data type: int, the quadrant that corresponds to the Axis 2 angle or the rounded-down joint angle.

cf3, data type: int, the quadrant that corresponds to the Axis 3 angle or the rounded-down joint angle.

cf4, data type: int, the quadrant that corresponds to the Axis 4 angle or the rounded-down joint angle.

cf5, data type: int, the quadrant that corresponds to the Axis 5 angle or the rounded-down joint angle.

cf6, data type: int, the quadrant that corresponds to the Axis 6 angle or the rounded-down joint angle.

cf7, data type: int, the quadrant that corresponds to the Axis 7 angle or the rounded-down joint angle.

cfx, data type: int, the configuration number of the form used by the robot, ranging from 0 to 8.

Example

There are different inverse kinematics for the same end-effector Cartesian space pose. The values of cfx from 0 to 8 represent each group of inverse kinematic solutions, which are explained in detail as follows.

For 6-axis industrial robots, xMateER collaborative robots, and 7-axis robots:

cfx

Wrist center is on Axis 1…​

Wrist center on the lower arm…

Wrist angle is…​

0

Front

Front

Positive

1

Front

Front

Negative

2

Front

Rear

Positive

3

Front

Rear

Negative

4

Rear

Front

Positive

5

Rear

Front

Negative

6

Rear

Rear

Positive

7

Rear

Rear

Negative

For xMateCR collaborative robots (cfx=0 represents the solution that is closer to the joint angle represented by cf1−6):

cfx

Wrist center is on Axis 1…​

Wrist center on the lower arm…

Axis 5 angle is…​

0

1

Front

Front

Negative

2

Front

Front

Positive

3

Front

Rear

Negative

4

Front

Rear

Positive

5

Rear

Front

Negative

6

Rear

Front

Positive

7

Rear

Rear

Negative

8

Rear

Rear

Positive

For xMateSR collaborative robots, cfx is always 0, indicating the solution that is closer to the joint angle represented by cf1−6.

For 3-axis industrial robots and 4-axis industrial robots:

cfx

Wrist center on the lower arm…

0

Front

1

Rear

15.1.10 jointtarget

Explanation

To store the robot’s joint angle and the positions of external axes.

Definition

robax, Robot Axis, data type: double, containing 7 members of double type, which store the angle of the robot’s 7 joints, in Degree.

extax, External Axis, data type: double, containing 6 members of double type, which can store the position of up to 6 external axes. If the external axis is a rotation axis, the unit is Degree; if the external axis is a linear axis, the unit is mm.

Example

In the variable list:

image736

The above command defines a point named "jointtarget0" in the joint space. Except that the Axis 6 is 90 degrees, the other axes of the robot are all 0 degrees. The first external axis is set to 10 degrees or 10 mm, depending on the type of external axis; the remaining external axes are set to zero.

Structure assignment

jointtarget j1 = J:{-268.649031, 321.536626, 259.344893, 55.143011, 66.111070, 169.543340, 29.916387}{EJ 0, 0, 0, 0, 0, 0};

Note:

  1. 1. J:{…​} represents the angles (in degrees) of the robot’s 7 joints, with each value being of type double.

  2. {EJ …​} defines the position information of 6 external axes, also of type double. In this example, all external axis values are set to 0.

15.1.11 load

Explanation

The variable type load is used to store the dynamic parameters of the robot’s load.

There are two main types of robot loads:

  • The tool or work object itself installed at the end-effector of the robot;

  • Objects that the tool picks up/sucks up.

The variable load does not support individual creation. It can only be manually modified in the tool calibration interface as a member of the tool-type variables or automatically modified by the control system using the load identification function.

By defining the dynamic parameters of the load correctly, the robot can achieve optimal performance. The wrong definition may lead to the following consequences:

  • The robot cannot maximize the ability to use the servo system, resulting in degraded performance.

  • The accuracy of the path is reduced, and the positioning error increases.

  • Overloading of mechanical components results in a reduction in life or damage.

Definition

In the xCore system, the load is treated as a rigid body. There are four parameters for describing the load:

mass, data type: double, the mass of the load, in kg.

cogx, the offset of the center of mass in the X-direction, data type: double, if the tool is mounted on the robot, cogx records the offset of the center of mass in the X direction of the tool frame; if the external tool function is used, the cogx records the offset of the center of mass of the load held by the gripper in the X direction of the work object frame.

cogy, the offset of the center of mass in the Y-direction, data type: double, if the tool is mounted on the robot, cogy records the offset of the center of mass in the Y direction of the tool frame; if the external tool function is used, the cogy records the offset of the center of mass of the load held by the gripper in the Y direction of the work object frame.

cogz, the offset of the center of mass in the Z-direction, data type: double, if the tool is mounted on the robot, cogz records the offset of the center of mass in the Z direction of the tool frame; if the external tool function is used, the cogz records the offset of the center of mass of the load held by the gripper in the Z direction of the work object frame.

q1~q4, quaternions, to record the direction of the principal axis of inertia of the load, data type: double;

When the tool is mounted on the robot, the orientation of the principal axis of inertia is described in the tool frame. See the figure below for details:

15.1.11 1

When using an external tool, the direction of the principal axis of inertia is described in the work object frame. See the figure below:

15.1.11 2

Ix, inertia x, data type: double, the inertia of the load along the x-axis, in kgm2.

Iy, inertia y, data type: double, the inertia of the load along the y-axis, in kgm2.

Iz, inertia z, data type: double, the inertia of the load along the z-axis, in kgm2.

Note: Correctly defining the load inertia helps to improve the robot’s movement accuracy, especially when handling large objects. If ix, iy, iz are set to zero, the load will be treated as a mass. Usually, if the distance from the center of mass of the load to the flange center point is smaller than the maximum size of the load itself, the load inertia should be defined, as shown in the following figure:

15.1.11 3

15.1.12 orient

Explanation

It is used to store the orientation information of the frame or space rigid body.

Variables of orient type do not support individual creation or modification and are only used as member variables of some variables.

Definition

The RL language system uses quaternions to represent orientations, so there are a total of 4 components expressed as follows:

q1, data type: double, the 1st component of the quaternion.

q2, data type: double, the 2nd component of the quaternion.

q3, data type: double, the 3rd component of the quaternion.

q4, data type: double, the 4th component of the quaternion.

Remarks

We usually describe the orientation of the rigid body by using the rotation matrix. The quaternion is another way to describe orientation more concisely.

The four components of the quaternion satisfy the following relationship:\(q_{1}^{2} + q_{2}^{2} + q_{3}^{2} + q_{4}^{2} = 1\)

The rotation matrix and the quaternion can be converted to one another. It is supposed that there is a rotation matrix R,

\$R = \begin{bmatrix} r_{11} & r_{12} & r_{13} \\$ \$r_{21} & r_{22} & r_{23} \\$ \$r_{31} & r_{32} & r_{33} \end{bmatrix}\$

then: 15.1.12 2

15.1.13 pos

Explanation

It is used to store location information in 3D space.

Variables of pos type do not support individual creation or modification and are only used as member variables of some variables.

Definition

The RL language system describes three-dimensional space using the Cartesian frame, so the pos variable has three components: x, y, and z.

X, data type: double, the X coordinate of the position.

Y, data type: double, the Y coordinate of the position.

Z, data type: double, the Z coordinate of the position.

15.1.14 pose

Explanation

It is used to store the position and orientation of Cartesian space.

Definition

X, data type: double, the X coordinate of the position.

Y, data type: double, the Y coordinate of the position.

Z, data type: double, the Z coordinate of the position.

Q1, data type: double, the 1st component of the quaternion.

Q2, data type: double, the 2nd component of the quaternion.

Q3, data type: double, the 3rd component of the quaternion.

Q4, data type: double, the 4th component of the quaternion.

Structure assignment

pose pose_obj = PE:{{X, Y, Z}, {Q1, Q2, Q3, Q4}};

Refer to the above definitions for parameter meanings.

Example: pose pose_obj = PE:{{100, 100, 100}, {1, 0, 0, 0}};

This struct supports the assignment of Euler angles. Please refer to the description of the robtarget structure for details.

15.1.15 robtarget

Explanation

It aims to store Cartesian positions and orientations of 3D space, which is used for MoveJ, MoveL, MoveC, and MoveT commands.

Because of the multi-solvability of the inverse kinematics of the robot, the robot can arrive in many different forms for the same target pose. In order to specify the configuration form, the robtarget variable also contains the robot configuration data.

Variables of the robtarget type are automatically created when the motion command is inserted by auxiliary programming. Manually changing the internal value of the variable may lead to non-correspondence between the Pose and ConfData, and the robot cannot execute the motion command normally.

Note: The use of Cartesian positions and orientations in robot programs is defined in the work object frame. If the work object used in the end is not the same as that used during the initial programming, the robot’s motion will deviate from the desired path. Therefore, it shall be confirmed that the changes in work object will not cause danger in the following two cases:

  • Use the "Modify Command" function to change the wobj parameter of the command;

  • The actual work object used is different from the one used in the program commands.

Improper use can result in personal injury or equipment damage!

Definition

Trans, spatial position, data type: pos, the position offset stored in the reference frame.

Rot, orientation, data type: orient, the orientation stored in the reference frame.

Conf, Robot Configuration Data, data type: confdata, to save the configuration data of the robot. Please refer to confdata for details.

Extax, External Axis, data type: double, containing 6 members of double type, which can store the position of up to 6 external axes. If the external axis is a rotation axis, the unit is Degree; if the external axis is a linear axis, the unit is mm.

Example

image737image738

A Cartesian space pose named p1 with the position and orientation (in quaternions) as shown above is defined. The elbow is 10°, and the angles of the Axis 1, 3, 5, and 7 are between 0 and 90°. The robot belongs to the first group of morphological configurations (see confdata for details), and all external axes are in zero.

Structure assignment

robtarget rob1 = p:{{849.572593, -347.654631, 35.341636}, {-0.361604, 0.078279, 0.640346, -0.673106}, -1.058584}{cfg 1, 2, 3, 4, 5, 6, 7, 8}{EJ 1, 2, 3, 4, 5, 6};

Explanation: p:{{Space Position Trans}, {Orientation Rot}, {Arm Angle}}{cfg: Robot Configuration Data Conf}{EJ: External Axis Information Extax};

Starting from version 3.2, the robtarget type supports direct assignment of Euler angles (i.e., A, B, C). In version 3.1 and earlier, it only supports quaternions (q1−q4) to set the rotation orientation.

Example code (pseudocode):

proc main()

robtarget p1;

//Version 3.1 and earlier: only support quaternion assignment

p1.rot.q1 = 1;

p1.rot.q2 = 0;

p1.rot.q3 = 0;

p1.rot.q4 = 0;

//Added in version 3.2: support Euler angle assignment

p1.rot.a = someVariable; //Variable

p1.rot.b = 90.0; //Constant

p1.rot.c = reg1; //Register

//Note: The data types of a, b, and c are double

endproc

Attention

Euler angle is in degrees (°)

When assigning to Euler angles, the assignment source can be a variable, constant, or register, as long as its value can be implicitly converted to a double type.

A robtarget maintains two sets of representations — Euler angles (A/B/C) and quaternions (q1−q4) internally. Whenever either representation is modified, the other one will be automatically synchronized and updated (provided that the data is valid).

Quaternion validity handling rules:

Quaternions must satisfy the normalization condition (the sum of squares is 1). After a single assignment, the system will perform a check: After the assignment of each component (q1, q2, q3, or q4), the system will check whether the current quaternion is valid:

If valid: The corresponding Euler angles (A/B/C) will be updated synchronously.

If invalid: The Euler angles will not be updated and will retain their previous values.

If the quaternion remains invalid after an overall assignment: Even after assigning all quaternion components, if the final quaternion still does not satisfy the normalization condition, the Euler angles will remain unchanged. In such cases, the system will perform a validity check when executing motion commands, and may either report errors or automatically normalize the quaternion (the specific behavior is determined by the motion command execution).

Explanation of Euler angle assignment behavior:

When assigning any component of a, b, or c, the system will immediately recalculate the corresponding quaternion based on the current complete Euler angle value and update rot. q1−q4.

The Euler angles derived from the quaternion will not override the Euler angle values explicitly set by the user. The original Euler angle values are also kept. This is because the two representations are mathematically equivalent, making redundant updates unnecessary.

15.1.16 signalxx

Explanation

signalxx type variables are used to describe I/O signals.

All signalxx type variables need to be defined in the "Input/Output" and then used in the program. Direct declaration in the program is not supported.

signalxx currently only supports digital input and output, including the following variable types:

15.2.16 1

The signaldo and signalgo types contain only signal references and can be assigned using separate commands (e.g., SetDO, SetGO, etc.).

signaldi and signalgi can be used to directly obtain the value of the corresponding input signal in the program.

Note:

  • It is not supported to define/declare variables of type signalxx in the program. If such usage occurs, the program will report an error. Before using variables of signalxx type, please configure them in the IO signal list.

  • The scope of the signalxx variable is System, and its priority, when compared with other scope types, is System > GLOBAL > LOCAL.

  • If the variables declared in the Signal of the IO configuration interface and in the RL programs have the same name, the variable of scope in a lower level will be selected.

Example

Example 1

//Use the state of the digital input as a criterion for judgment

IF (di1 == true)

do something…

ENDIF

Example 2

//Use the state of the digital input as a criterion for judgment. For example, if the definition group input gi2 maps the first three bits of the 1st byte of Profinet IO, then when the values of bit0 to bit2 are 0, 1, and 1, the value of gi2 is 110 (6 after being converted to int). The same goes for group output (signalgo) as well.

IF (gi2 == 6)

do something…

endif

15.1.17 speed

Explanation

It is used to define the speed of the robot and the external axes.

Definition

The speed-type variable contains 5 member variables: Joint Velocity Percentage, TCP Linear Velocity, Orientation Velocity, External Axis Linear Velocity, and External Axis Angular Velocity.
Joint Velocity Percentage, data type: double, to specify the motion speed when the joint movement command is applied, applicable to the commands MoveAbsJ and MoveJ, with the value ranging from 1% to 100%.
TCP Linear Velocity, data type: double, to define the linear velocity of the TCP, with the value ranging from 0.001 mm/s to 7000 mm/s.
Orientation Velocity, data type: double, to define the rotation speed of the tool, with the value ranging from 0.001 degrees/s to 500 degrees/s.
External Axis Linear Velocity, data type: double, to define the motion speed of the external linear axis, with the value ranging from 0 mm/s to 5000 mm/s.
External Axis Angular Velocity, data type: double, to define the motion speed of the external rotary axis, with the value ranging from 0 degrees/s to 1000 degrees/s.

Example

In the variable list:
image739
The image above shows a definition of a speed variable named speed0, in which the joint rotation speed is 40% of the maximum allowable speed, the TCP linear speed is 300 mm/s, the space rotation speed is 100°/s, the external axis angular velocity is 1000°/s, and the external axis linear velocity is 200 mm/s.

Structure assignment

speed speed0 = v:{40, 300, 100, 1000, 200};
Explanation: The image above shows a definition of a speed variable named speed0, in which the joint rotation speed is 40% of the maximum allowable speed, the TCP linear speed is 300 mm/s, the space rotation speed is 100°/s, the external axis angular velocity is 1000°/s, and the external axis linear velocity is 200 mm/s.

Name

Joint Velocity Percentage

TCP Linear Velocity

Orientation Velocity

External Axis Angular Velocity

External Axis Linear Velocity

v5

1%

5 mm/s

200°/s

5°/s

2 mm/s

v10

3%

10 mm/s

200°/s

10°/s

5 mm/s

v25

5%

25 mm/s

200°/s

25°/s

12 mm/s

v30

5%

30 mm/s

200°/s

30°/s

15 mm/s

v40

5%

40 mm/s

200°/s

40°/s

20 mm/s

v50

8%

50 mm/s

200°/s

50°/s

25 mm/s

v60

8%

60 mm/s

200°/s

60°/s

30 mm/s

v80

8%

80 mm/s

200°/s

80°/s

40 mm/s

v100

10%

100 mm/s

200°/s

100°/s

50 mm/s

v150

15%

150 mm/s

200°/s

150°/s

75 mm/s

v200

20%

200 mm/s

200°/s

200°/s

100 mm/s

v300

30%

300 mm/s

200°/s

300°/s

150 mm/s

v400

40%

400 mm/s

200°/s

400°/s

200 mm/s

v500

50%

500 mm/s

200°/s

500°/s

250 mm/s

v600

60%

600 mm/s

200°/s

600°/s

300 mm/s

v800

70%

800 mm/s

200°/s

800°/s

400 mm/s

v1000

100%

1000 mm/s

200°/s

1000°/s

500 mm/s

v1500

100%

1500 mm/s

200°/s

1500°/s

750 mm/s

v2000

100%

2000 mm/s

200°/s

2000°/s

1000 mm/s

V3000

100%

3000 mm/s

200°/s

3000°/s

1000 mm/s

v4000

100%

4000 mm/s

200°/s

4000°/s

1000 mm/s

vmax

100%

-

-

-

The system predefines some common speed variables, as shown in the following table.

All space rotation speeds in the system’s pre-defined speed variable are 200°/s. If there are special requirements on the rotation speed of the end-effector of the robot, a new speed variable can be defined for use according to the process requirements.

vmax is the only predefined parameter that can be configured by the user, and the modification method is described in 8.4.6.

15.1.18 tool

Explanation

The tool-type variables are used to record tool parameters, including TCP, orientation, and dynamic parameters of the tools used by the robot.

The robot uses tools to interact with the outside world, so the tool variable will affect the motion of the robot from the following aspects:

Only the TCP will move according to the programmed path and speed. When the robot executes a pure spatial rotation, only TCP will remain motionless;

The motion path and speed specified during programming refer to the path and speed of the tool frame relative to the work object frame. Therefore, replacing a well-calibrated tool or work object does not affect the shape and speed of the path;

When using external tools, the speed of programming refers to the speed of a work object (relative to external tools).

Note that when using the external tool, tframe in the tool-type variable will record the zero position and orientation offset of the external tool, while tload will record the dynamic parameters of the gripper that is installed at the end-effector of the robot for grasping work object.

The data of the tool-type variable is stored in the database. When the program is loaded, it is read by the program editor from the database. Therefore, do not try to modify the tool-type variable directly in the program editor, and thus the unpredictable errors will be avoided. If you need to modify the tool-type variable, please modify it through the calibration interface. See the Calibration of the tool frame for details.

Be sure to correctly define the dynamic parameters of the end-effector load of the robot, including the tool itself and the two parts of the object captured by the tool. The wrong definition may lead to the following consequences:

  • The robot cannot maximize the ability to use the servo system, resulting in degraded performance;

  • The accuracy of the path is reduced, and the positioning error increases;

Overloading of mechanical components results in a reduction in life or damage.

Example

Robhold, data type: boot, to define whether the tool is installed on the robot. True indicates that the tool is installed on the robot. False indicates that the tool is not installed on the robot and an external tool is being used. When making a jog or executing a program, only one of the robhold parameters can be True in the tool/work object combination used at the same time. That is, if the robhold of the tool is True, the corresponding work object robhold must be false, and vice versa; otherwise, the robot will prompt an error, and it is impossible to make a jog or execute the corresponding program command.

Tframe, Tool Frame, data type: pose, to record the tool frame of the tool used, including:

TCP represents the offset in the x, y, and z directions relative to the robot end-effector flange frame, in millimeters. The orientation offset of the tool frame relative to the flange frame is expressed in quaternion. See the following figure for details:

15.1.18.1 15.1.18.2

Tload, dynamic parameters of the tool, data type: load, to record the dynamic parameters of the tool. For the common tool, tload describes the dynamic parameters of the entire tool. For external tools, tload describes the dynamic parameters of the gripper used by the robot (holding the work object). For general tools installed on the robot, the load parameters include:

The mass of the tool (weight), in kg;

The center of gravity of the tool, described in the flange frame, in millimeters (mm); the direction of the principal axis of inertia, described in the flange frame; and

The inertia magnitude of the tool along the principal axis of inertia, in kgm2. If all inertia components are defined as 0 kgm2, the tool is treated as a Point Mass.

Note:

When using the external tool function, the TCP and orientation are defined relative to the world frame.

If the robot is using an external tool, then the tload member is used to record the dynamic parameters of the gripper installed on the robot. The meaning of the specific parameters remains unchanged.

Please note that the tload members only define the dynamic parameters of the gripper used by the robot (holding the work object). The dynamic parameters of the gripped work object are not included. To ensure that the robot performs optimally under all circumstances, you need to define two tool variables to handle this situation:

  • A tool saves all parameters of the gripper itself;

  • Another tool saves all parameters of the gripper + gripped work object;

The use of different tools in the motion command would help implement the switching function with or without load.

Structure assignment

tool tool0 = {whether the tool is handheld, {{tool position}, {tool orientation quaternion}}, {mass, {center of gravity X, center of gravity Y, center of gravity Z}, {load orientation quaternion}, inertia ix, inertia iy, inertia iz}};

whether the tool is handheld: true, handheld; false, external.

tool tool0 = {Example:true, {{0, 0, 0}, {1, 0, 0, 0}}, {0, {0, 0, 0}, {1, 0, 0, 0}, 0, 0, 0}};

This struct supports the assignment of load Euler angles. Please refer to the description of the robtarget structure for details.

15.1.19 Trigdata

Explanation

trigdata is used to store information data about the trigger events during robot motion, including trigger conditions and trigger actions.

The trigger condition is usually reaching a specified location on the path; the trigger action can be setting IO, setting variables, etc.

Variables of type trigdata cannot be defined by the assignment operator and can only be defined by a specific RL command, so the information stored in each trigdata variable depends on the Trig command as used, for example, the TrigIO, etc.

Then, it can be used by the corresponding movement commands TrigL, TrigC, TrigJ, etc.

Example

The following example shows how to use the trigdata:

Example 1

VAR trigdata gripopen;

TrigIO(gripopen, 0.5, do1, true);

TrigL(p1,v500, gripopen, fine, tool1);

15.1.20 wobj

Explanation

wobj is an abbreviation for Work Object. Work object refers to an object processed, handled, or transported by a robot.

All the positions used in the motion command are defined in the work object frame (if no work object frame is specified, it defaults to the world frame. The world frame can be seen as a wobj0). There are several benefits in doing this:

  • The location of many processing points can be obtained from the design drawing of the work object and used directly;

  • When the robot is reinstalled or the work object is moved, you only need to re-calibrate the work object frame to reuse the previous program and avoid reprogramming.

  • With a suitable sensor provided, vibrations or slight movements of the work object can be automatically compensated.

Under normal circumstances, if you do not define a specific work object frame, the control system will then regard the world frame as the default work object frame wobj0. However, when using external tools, the work object frame must be defined because the programming path and speed refer to the path and speed of the work object, rather than the tool.

Usually, the work object frame is defined relative to the user frame, but if the user does not specify a user frame, the work object frame is defined by default relative to the world frame. For details, see the Robot’s frames.

The work object actually consists of two frames, the user frame and the work object frame. Inserting a user frame at the upper layer of the work object frame is to support the situation where multiple identical work objects need to be machined. For an explanation of the defining relationships of the relevant coordinates, see the explanation of oframe in the "Definitions" section.

Definition

Robhold, to define whether the work object is mounted on the robot. True indicates that the work object is mounted on the robot and the external tool is currently being used. False indicates that the work object is not mounted on the robot and the normal tool is currently being used.

Ufprog, User Frame Programmed, data type: bool, to define whether the user frame is fixed or moving. True indicates that the user frame is fixed, False indicates that the user frame is moving, e.g., to define whether it is on an external positioner or another robot.

This value is mostly used when the robot is required to coordinate its movement with the positioner or other robots.

Ufmec, User Frame Mechanical Unit, data type: string, the mechanical unit name is used to specify which mechanical unit the user frame is bound to; it is useful only if ufprog is false.

Oframe, Work Object Frame, data type: pose, to store the origin and orientation of the work object frame.

uframe_id, User Frame ID, data type: int, to store the id of the user frame. The corresponding user frame can be found by id.

When using normal tools (non-external tools), the frame definition chain is as follows: The work object frame is defined relative to the user frame; the user frame is defined relative to the world frame.

15.1.20.1

When using external tools, the frame definition chain is as follows: The work object frame is defined relative to the user frame; the user frame is defined relative to the flange frame.

15.1.20.2

Structure assignment

wobj wobj0 = {Robhold, Ufprog, Ufmec, Oframe, uframe_id, { mass, {center of gravity X, center of gravity Y, center of gravity Z}, {load orientation quaternion}, inertia ix, inertia iy, inertia iz }};

Refer to the "Definition" section of this table for parameter meanings.

wobjExample: wobj0 = {false, true, "robot", {0, 0, 0}, {1, 0, 0, 0}, 0, {0, {0, 0, 0}, {1, 0, 0, 0}, 0, 0, 0}};

This struct supports the assignment of load Euler angles. Please refer to the description of the robtarget structure for details.

15.1.21 zone

Explanation

The zone variable is used to define how a certain motion ends, or to define the size of the turning zone between two motion trajectories.

For the same target point of robot commands, there are two processing methods in the motion command:

  • When it is processed as a stop-point, the robot will move to the target point and reach the target point at a speed of 0 before continuing to execute the next command;

  • When it is processed as a transition point, the robot will not move to the target point but will start proceeding to the next target point at a place that is several millimeters away from such a target point. The turning path will deviate from the programmed path. We call the transition area between the two trajectories a turning zone. See the following figure for details:

15.1.21

The size of the turning zone cannot exceed half of the path length. If it is exceeded, the system will automatically reduce the turning zone to half the total path length. The use of turning zones prevents the robot from starting and stopping frequently, significantly reducing the cycle time.

Note:

In some special cases, the turning zone will be canceled. The system will report the log "Corner Path Failed". Possible causes are as follows

  • Turning zone length too small (0.01 mm/0.00001 rad);

  • At least one of the two trajectories is too short (1 mm/0.001 rad);

  • The two trajectories are nearly parallel and the direction of motion is opposite;

  • The two trajectories perform pure rotation with the motion axis reversed. Such that only the end-effector axis rotates forward in the previous trajectory, and only the end-effector axis rotates reverse in the latter trajectory.

  • When a warning for "Turning Zone Canceled" is generated, the program automatically treats the affected command target point as a stop-point.

  • In addition to the special cases above, all logic commands will cancel the turning zone of the previous motion command.

Definition

Joint space trajectories and Cartesian space trajectories define turning zones with different parameters. The variable contains two parts: distance and percent.

Distance, size of turning zone in Cartesian space, data type: double; it is used for the commands MoveL, MoveC, and MoveT to define the size of the turning zone for Cartesian space trajectories, that is, when the robot moves to a point with a distance of several millimeters to the target point, it starts to move to the next target point, in millimeters, with the value ranging from 0 to 200 mm.

Percent, turning percentage, data type: double; it is used for MoveJ and MoveAbsJ, indicating how far it is to the target angle when starting turning. 100% represents half the value of the entire rotation angle. For command MoveL with pure space-rotation, the parameter Percent is used instead of Distance.

Example

In the variable list:

image740

A zone variable is defined, in which the size of the Cartesian turning zone is 100 mm and the size of the joint space turning zone is 50%.

Structure assignment

zone z1 = s:{Distance, Percent};

Refer to the "Definition" section of this table for parameter meanings.

zone z1 = Example:s:{1, 1};

The system predefines some common turning zone variables, as shown in the following table.

Name

Size of turning zone in Cartesian space

Turning percentage

fine

0 mm

0%

z0

0.005 mm

0.0005%

z1

1 mm

1%

z5

5 mm

3%

z10

10 mm

5%

z15

15 mm

8%

z20

20 mm

10%

z30

30 mm

15%

z40

40 mm

20%

z50

50 mm

25%

z60

60 mm

30%

z80

80 mm

40%

z100

100 mm

50%

z150

150 mm

75%

z200

200 mm

100%

15.1.22 torqueinfo

Explanation

It is used to describe the forces and torques applied to the robot;

It includes joint space torque information and Cartesian space torque information;

Definition

joint_torque, data type: joint space torque information;

cart_torque, data type: Cartesian space torque information;

joint_torque.measure_torque, data type: double array, information of measured force in the joint space and the torque applied to each axis measured by the force sensor;

joint_torque.external_torque, data type: double array, information of external force in the joint space, and information of the torque applied to each axis measured by the controller based on the robot model and measured force;

cart_torque.m_force, data type: double array, force in all directions (xyz) in the Cartesian space;

cart_torque.m_torque, data type: double array, torque in all directions (xyz) in the Cartesian space;

Example

The following example shows how to use variable torqueinfo:

Example 1

TorqueInfo tmp_info = GetEndtoolTorque(tool1, wobj1);

//Obtain the information architecture of the torque applied to the tool at the end-effector of the robot in the case of tool1 wobj1

…

print(tmp_info.joint_torque.measure_torque);

print(tmp_info.joint_torque.external_torque);

//Print the measured force and external force of each axis

…

print(tmp_info.cart_torque.m_torque);

//Print Cartesian space torque

…

print(tmp_info.cart_torque.m_force);

print(tmp_info.cart_torque.m_torque);

//Print information of force and torque in X direction

15.1.23 SocketServer

Explanation

A Socket TCP server is established on the controller to listen for connections initiated by external devices as the client. This server is only used to listen for connection requests and multiple connections are supported. When a connection is established, a new SocketConn object is generated for communication.

Note:

  • Do not create (OpenDev) and destroy (CloseDev) server resources too often as it requires time for system resource application and release. It is recommended to keep at least a 500 ms time interval between creating and destroying resources; otherwise, system resources will be overloaded and cause problems.

  • This command only creates a server resource object, and the server creation is not completed. The server needs to enter the listening state via OpenDev and SocketAccept.

  • The server supports multiple connections.

Definition

Ip, data type: string; the control system uses the ip parameter to match the network interface controller (NIC) and uses the corresponding NIC for network listening. If this parameter is set to "0.0.0.0", it means listening for the connections of all NICs. In most cases, it can be set to "0.0.0.0".

Port, data type: int, listening port. When an external client initiates a connection, specify the value of the server port set for this purpose.

Name, data type: string, the unique identifier of the server used in the RL program. It is unique within the project and can be shared between multiple tasks without naming conflicts.

Example

Example 1

SocketServer ss = {"192.168.0.160", 8090, "svr"};

//Only listen for NIC with ip set to 192.168.0.160

SocketConn conn = SocketAccept( "svr");

Example 2

SocketServer ss = {"0.0.0.0", 8090, "svr"} ; //Listen for all NICs of the robot

SocketConn conn = SocketAccept( "svr");

15.1.24 SocketConn

Explanation

Socket TCP connection object, used for communication to external devices. There are two types:

  • The robot, as a client, initiates a connection and communication through the object to the TCP server of the external device.

  • The robot acts as a server for communication connections to the counterpart device generated when a connection is initiated by a TCP client of the external device. When multiple TCP client connections are initiated by different external devices, one connection is generated for each connection.

Definition

Ip, data type: string; when the robot is used as a client, this parameter indicates the ip of the external device’s server. When the robot is used as a server, this parameter indicates the ip of the external client when a connection is established by the external device.

Port, data type: int, listening port. When the robot initiates a connection, the server port of the external device should be specified.

Name, data type: string, the unique identifier of the connection used in the RL program. It is unique within the project and can be shared between multiple tasks among connections and between connection and server. Server names should not conflict within the project.

Cache, data type: int, size of the cache, indicating max data received that can be cached; it can be left blank. 1 by default.

Suffix, data type: string, terminator, indicating the end of a message; it can be left blank. "+r" by default.

Attr, data type: string, connection attribute.

  • "incoming": local server, connected by the opposite-end client. ip and port identify the client information.

  • "outgoing": local client, connected to the external server. ip and port identify the opposite-end server connected.

  • "" and others: unavailable connection, indicating that the connection has not been opened or unestablished connection has been found.

State, data type: string, current communication connection status; closed: connection closed; established: connection established and working properly.

Note:

  • When used as a client, the ip and port information should be set by the user. When used as a server, the ip and port information should be automatically obtained from the accept command. Do not modify these two values easily after the connection is established, unless you are very clear about the use of these two values to avoid errors in program logic and operation.

  • suffix can be reset at any time and can take effect until the next read. Use this feature with caution, as it can cause communication data errors. suffix should be set before communication and should not be modified again.

Example

Example 1

//Server ip "192.168.0.202", port 8090, connection name "clt", cache default to 1, and suffix default to "+r"

SocketConn scnn1 = {"192.168.0.202", 8090, "clt"};

Example 2

//Server ip "192.168.0.203", port 8091, connection name "clt1", cache 2, and suffix default to "+r"

SocketConn scnn2 = {"192.168.0.203", 8091, "clt1", 2};

Example 3

//Server ip "192.168.0.204", port 8092, connection name "clt2", cache 2, and suffix "+n"

SocketConn scnn3 = {"192.168.0.204", 8092, "clt2", 2, "+n"};

Example 4

//Used as server, connection established by the external device

//Server ip "192.168.0.204", port 8092, connection name "clt2", cache 2, and suffix "+n"

SocketConn conn = SocketAccept( "svr1");

Print(conn.ip); //ip of the external device

Print(conn.port); //Port of the external device to establish the connection

Print(conn.cache); //Buffer queue for receiving messages

Print(conn.suffix); //Sending and receiving suffix

15.1.25 FCBoxVol

Explanation

It is used to define a spatial cuboid for position monitoring or termination conditions after force control is enabled.

Definition

Xmax represents the coordinate value of the cuboid boundary in the positive x direction;

Xmin represents the coordinate value of the cube boundary in the negative x direction;

Ymax represents the coordinate value of the cuboid boundary in the positive y direction;

Ymin represents the coordinate value of the cube boundary in the negative y direction;

Zmax represents the coordinate value of the cuboid boundary in the positive z direction;

Zmin represents the coordinate value of the cube boundary in the negative z direction;

Example

image741

Structure assignment

FcBoxVol fcboxvol0 = FCBV:{Xmin, Xmax, Ymin, Ymax, Zmin, Zmax};

Refer to the "Definition" section of this table for parameter meanings.

Example: FcBoxVol fcboxvol0 = FCBV:{0, 1, 2, 3, 4, 5};

15.1.26 FCSphereVol

Explanation

It is used to define a spatial sphere for position monitoring or termination conditions after force control is enabled.

Definition

Xc: the coordinate value of the center of the spatial sphere in the x direction;

Yc: the coordinate value of the center of the spatial sphere in the y direction;

Zc: the coordinate value of the center of the spatial sphere in the Z direction;

Radius: the spatial sphere radius;

Example

image742

Structure assignment

FcSphereVol fc = FCSV:{xc, yc, zc, radius};

Refer to the "Definition" section of this table for parameter meanings.

FcSphereVolExample: fc = FCSV:{1, 2, 3, 4};

15.1.27 intnum

Explanation

Used as an interrupt identifier. An intnum variable can only identify one interrupt.

Definition

Example

image743