Skip to main content

Dependencies and Environment

Compatibility​

HMI Plugin uses QT/C++ as the basic development language, and the program is designed according to the C++11 standard.

HMI Plugin supports Qt version 5.12 and above.

*** To ensure that secondary development plugins can be loaded and run normally, it is recommended to use the recommended compiler and runtime environment ***

Compilation and Environment​

Library NameOperating SystemCompilerPlatform
libxplugin.soUbuntu 18.04GNU Compiler Collection 9.4aarch64
libxplugin.soUbuntu 18.04gcc-linaro-6.3.1-2017.05-x86_64_aarch64-linux-gnux86_64 for Linux
xplugin.dll, xplugin.libWindows 10/11MSVC2017x86_64 for Windows

To facilitate user development, Rokae provides a virtual machine development environment. Users can download this environment from the official website and run the Controller in the virtual machine.

Contact Rokae official technical support to obtain the virtual machine usage process.