Data Structures
1 Robot Basic Info Info
str id # Robot uid, can be used to distinguish connected robots
str mac # MAC address
str version # Controller version
str type # Robot model name
int joint_num # Number of axes
2 Frame Frame
list[float] trans # Translation, [X, Y, Z], unit: meter
list[float] rpy # XYZ Euler angles, [A, B, C], unit: radian
list[float] pos # Row-major homogeneous transformation matrix.
3 Cartesian Position CartesianPosition
Inherits Finishable.
list[float] trans # Translation, [x, y, z], unit: meter
list[float] rpy # XYZ Euler angles, [A, B, C], unit: radian
float elbow # Elbow angle, applicable to 7-axis robots, unit: radian
bool hasElbow # Whether has elbow angle
list[float] confData # Axis configuration data, number of elements should match robot axes
list[float] external # External joint values, unit: radian|meter. Rail unit is meter
4 Cartesian Position Offset CartesianPositionOffset
CartesianPositionOffsetType type # none: no offset; offs: workpiece frame; relTool: tool frame
Frame frame # Frame offset (should be Frame type object)
5 Joint Position JointPosition
Inherits Finishable.
list[float] joints # Joint angle values, unit: radian
list[float] external # External joint values, unit: radian|meter. Rail unit is meter
6 Joint Torque, Excluding Gravity and Friction Torque
Inherits Finishable.
list[float] tau # Desired joint torque, unit: Nm
7 Load Info Load
float mass # Load mass, unit: kilogram
list[float] cog # Center of gravity [x, y, z], unit: meter
list[float] inertia # Inertia [ix, iy, iz], unit: kilogram·square meter
8 Tool Workpiece Set Info Toolset
Calculated based on a pair of tool workpiece coordinates, load, and robot handheld settings.
Load load # Robot end handheld load
Frame end # Robot end frame relative to flange frame transformation
Frame ref # Robot reference frame relative to world frame transformation
9 Frame Calibration Result FrameCalibrationResult
Frame frame # Calibration result (Frame type object)
list[float] errors # Deviation between sample points and TCP calibration value,依次为 minimum, average, maximum, unit m
10 RL Project Info RLProjectInfo
str name # Project name
list[str] taskList # Task name list
11 Tool/Workpiece Info WorkToolInfo
str name # Name
str alias # Description
bool robotHeld # Whether robot handheld
Frame pos # Pose. Workpiece frame has been transformed relative to its user frame (Frame type object)
Load load # Load (Load type object)
12 Motion Command MoveAbsJ MoveAbsJCommand
JointPosition target # Target joint position (JointPosition type object)
int speed # End linear velocity, unit mm/s, joint velocity is divided into several intervals based on end linear velocity size, see setDefaultSpeed() for details
float jointSpeed # Joint speed ratio, range [0, 1]. Takes effect when >= 0; when < 0, the joint speed derived from speed is used
int zone # Zone size, unit mm
str customInfo # Custom info, can be returned in motion info feedback
13 Motion Command MoveJ MoveJCommand
CartesianPosition target # Target Cartesian position (CartesianPosition type object)
int speed # End linear velocity, unit mm/s, joint velocity is divided into several intervals based on end linear velocity size, see setDefaultSpeed() for details
float jointSpeed # Joint speed ratio, range [0, 1]. Takes effect when >= 0; when < 0, the joint speed derived from speed is used
int zone # Zone size, unit mm
CartesianPositionOffset offset # Offset (CartesianPositionOffset type object)
str customInfo # Custom info, can be returned in motion info feedback
14 Motion Command MoveL MoveLCommand
CartesianPosition target # Target Cartesian position (CartesianPosition type object)
int speed # End linear velocity, unit mm/s
float rotSpeed # Spatial rotation speed, unit rad/s. Takes effect when >= 0; defaults to 200°/s when < 0
int zone # Zone size, unit mm
CartesianPositionOffset offset # Offset (CartesianPositionOffset type object)
str customInfo # Custom info, can be returned in motion info feedback
15 Motion Command MoveC MoveCCommand
CartesianPosition target # Target Cartesian position (CartesianPosition type object)
CartesianPosition aux # Auxiliary position (CartesianPosition type object)
int speed # End linear velocity, unit mm/s
float rotSpeed # Spatial rotation speed, unit rad/s. Takes effect when >= 0; defaults to 200°/s when < 0
int zone # Zone size, unit mm
CartesianPositionOffset targetOffset # Target point offset (CartesianPositionOffset type object)
CartesianPositionOffset auxOffset # Auxiliary point offset (CartesianPositionOffset type object)
str customInfo # Custom info, can be returned in motion info feedback
16 Motion Command MoveCF MoveCFCommand
target and aux are constructor arguments only; they are not exposed as attributes. rotSpeed and point offsets are not bound either. Accessible fields (speed, zone, and customInfo are inherited from NrtCommand):
float speed # Max end linear velocity, unit mm/s
int zone # Zone radius, unit mm
str customInfo # Custom info, returned in motion feedback
float angle # Full circle execution angle, unit: radian
MoveCFCommandRotType rotType # Full circle orientation rotation mode
17 Motion Command MoveSP MoveSPCommand
CartesianPosition target # End Cartesian position; only rpy is used to set the end orientation (CartesianPosition type object)
CartesianPositionOffset targetOffset # Offset option (CartesianPositionOffset type object)
float radius # Initial radius, unit: meter
float radius_step # Radius change per unit angle, unit: meter/radian
float angle # Total rotation angle, unit: radian
bool direction # Rotation direction, true - clockwise | false - anticlockwise
str customInfo # Custom info, can be returned in motion info feedback
18 Motion Wait Command MoveWaitCommand
float duration_ # Wait duration, minimum effective duration 1ms
19 Controller Log Info LogInfo
int id # Log ID number
str timestamp # Date and time
str content # Log content
str repair # Repair method
20 End Keypad State KeyPadState
bool key1_state # CR1 number
bool key2_state # CR2 number
bool key3_state # CR3 number
bool key4_state # CR4 number
bool key5_state # CR5 number
bool key6_state # CR6 number
bool key7_state # CR7 number
21 CAN Frame CANFrame
int frame_id # Frame ID
int frame_format # Frame format (see CANFormat)
int frame_type # Frame type (see CANType)
list[int] data # CAN data (interpreted by data_type as uint8/int16/uint16)
int frame_valid_length # Valid length (element count; must equal len(data))
22 Single-Group CAN Send/Receive Parameters CANRwItem
can_id: int CAN frame ID
can_format: int Frame format (see CANFormat)
can_type: int Frame type (see CANType)
send_len: int Number of bytes to send, must equal len(send_data)
rev_frames_per: int Expected receive frame count. Each group sends one frame and expects one frame if this value is 1, or multiple frames if it is greater than 1.
send_data: list[int] Raw bytes to send
23 CAN Send/Receive Request CANRwParam
interval_ms: int Interval between send/receive groups in ms. Use 0 for no wait.
rw_frames: list[CANRwItem] Send/receive sequence