Skip to main content

8.10 IO signal list

8.10.1 Overview

In addition to the default Universal IO signals created by the "IO device" in the enabled state, if you want to use the IO device alone to create a user IO signal, you need to create it on the "IO Signal List" page.

The signalxx type variables are used to store and access IO signals in the RL program. For details, refer to relevant sections about RL commands.

image329

①

IO signal list, where you can view IO signal attributes, including:

* Signal name;
* Type: including DI/DO/GI/GO;
* IO board: It can be a standard IO module provided by ROKAE, and can also be a Profinet bus or Ethernet/IP bus device;
* Start port and end port: the corresponding physical address that a IO signal mapped.

②

Function button area, where you can import, export, create, edit, multi-select, and delete IO signals

  1. If there is an error in the IO configuration, for example, when the mapped IO port exceeds the physical limits or the IO is repeatedly assigned, the controller system will enter the SYS_ERR state at the system starting and give an alarm message on the HMI. In this case, the user is only allowed to enter the system configuration interface to correct the wrong configuration, with no other operation allowed.

  2. The xCore system enables the mapping of both user IO and system IO to the same port. However, users are not allowed to write on the ports/signals that have been bound to system IO. That is, the signals mapped to the same port as the system IO are read-only for the users.

The configured IO can be viewed on the status monitoring interface, on which the forced output or simulation input of the IO is supported.

image330

8.10.2 Operation examples

Operation

Graphical Representation

Explanation

1. Click the "+" button in the lower right corner to create a new IO.

image331

Users with the permission level of "Programmer" or above can perform creation and edit operations.

2. Attribute settings.

image332

Set IO signal name, description, IO board, signal type, and port.

3. Using IO Signal in the RL program.

image333

image334

For the input signal (DI/GI), the state of the input node can be read directly in the RL program using the variable name of the input signal.

For example: Use the state of the digital input as a criterion for judgment

IF (di1 == true)

do something…

ENDIF

For the output signal (DO/GO), specialized commands SetDO and SetGO can be used in the RL program. See the Explanation of each command below for details.

8.10.3 IO signal export/import

8.10.3.1 IO signal export

On the IO signal list page, click theimage269 button at the bottom left to enter the IO signal export interface.

8.10.3.1

①

IO signal export target file (including path)

②

Filter box

③

IO signal list

④

IO signal export button

Export steps: First, input or select the path for the IO signal export target file in ①, and filter by name in ②, if necessary. Then, check the IO signals to be exported in ③. Finally, click the button in ④ to execute the export, and the exported IO signal file will be generated in the path specified in ①.

8.10.3.2 IO signal import

On the IO signal list page, click theimage::en/image271.png[width=700,align=center] button at the bottom left to enter the IO signal import interface.

8.10.3.2

①

IO signal import file

②

IO signal import option, which is the strategy for handling entry conflict

③

Filter box

④

IO signal import entry

⑤

IO signal import button

Import steps: First, select the IO signal file to be imported in ①, and filter by name in ③, if necessary. Then, select the conflict handling strategy in ② and the IO signals to be imported in ④. Finally, click the "Finish" button in ⑤ to execute the import, and the selected IO signals will be imported locally.