Errors and abnormal behavior
Motion start phase
Slight sag when motion starts
@control
Errors when starting motion
Errors during motion
How to catch motion errors
void funRTControl() {
try {
auto rtCon = robot.getRtMotionController().lock();
rtCon->startMove(RtControllerMode::jointPosition);
// Option A: blocking loop — errors throw during motion
rtCon->startLoop(true);
// Option B: non-blocking — errors throw at stopLoop
rtCon->startLoop(false);
rtCon->stopLoop();
} catch (const std::exception &e) {
std::cerr << e.what();
}
}
Causes and handling
Real-time mode defines 20 error types.
kInstabilityDetection
If this occurs often, raise the network tolerance with setRtNetworkTolerance while real-time mode is off; 60% or higher is recommended.
Velocity / acceleration over threshold
- If it stops right after
startMove, the start pose is usually not the current pose. - If it happens mid-motion, check host real-time behavior and network jitter.
- For custom trajectories, adjacent commands are often too far apart — improve planning.
- With switches or complex paths, try a direct cable first.
How to set the start pose correctly
For MoveJ(start_pos, target_pos, speed), obtain start_pos as follows:
- Recommended: read with
posture()/jointPos().
std::array<double, 16> init_position{};
Utils::postureToTransArray(
robot.posture(rokae::CoordinateType::flangeInBase, ec),
init_position);
- Loop
updateRobotStateto drain stale frames and read the latest state.
while (robot.updateRobotState(chrono::steady_clock::duration::zero()));
- Read and update the start pose on the first callback frame.
std::function<CartesianPosition()> callback = [&, rtCon]() {
if (init) {
robot.getStateData(RtSupportedFields::tcpPose_m, init_pos);
init = false;
}
};
rtCon->setControlLoop(callback, 0, true);
Noise or jitter during position control
@control
What to do
- When running SDK examples:
- Enable filtering (
setFilterFrequency,setFilterLimit). - Windows usually needs stronger filtering.
- Prefer a direct link to reduce network jitter.
- NIC choice affects real-time behavior (field feedback: Realtek often more stable).
- Enable filtering (
- For custom planning:
- In addition to the above, check callback overrun (cycle longer than 1 ms).
- If needed, verify the velocity profile is smooth.
For teach-pendant scope, callback timing, and follow lag, see Other usage and real-time topics.
How to view diagnostic data
Diagnostic curve meanings (added in v4.0 controller)
Command values
- rci_q_c: In joint-position mode, the commanded joint position sent by the user (use this to check whether the command is smooth)
Measured values
- rci_q_m: Current measured joint-space position
- rci_cart_m: Current measured Cartesian pose
- rci_qv_m: Current measured joint-space velocity
- rci_cart_v_m: Current measured Cartesian velocity
Filtered values
- rci_q_c_hw: Joint-space commanded position after filtering, then sent to the servo; the filter cutoff is controlled by
rtCon->setFilterFrequency - rci_cart_c_hw: Cartesian commanded position after filtering, then sent to the servo; the filter cutoff is controlled by
rtCon->setFilterFrequency