Skip to main content

8.14 Variable monitoring selection interface

8.14.1 Overview

The variable monitoring selection interface is used to add variables that need to be monitored.

8.14.1

①

Monitored variable filter: Filter to display only the monitored variables needed to be displayed in the list below.

②

Variable monitoring display: Show attributes of each variable, including name, scope, type, original dimension, and description.

③

Function button area: image384import monitored variables, image385export monitored variables, image386batch add, image387single add, image388delete monitored variables.

8.14.2 Operation examples

8.14.2.1 Batch add monitored variables

Operation

Graphical Representation

Explanation

1. Click the "Batch Add" button

8.14.2.1 1

Enter the variable selection interface.

2. Select the variables you need to monitor, check the boxes within the red frame, and then click the "Complete" button.

8.14.2.1 2

Note: When the monitored variable is an array, all elements within the array will be monitored after batch addition.

3. Open the Variable Monitoring in Status Monitoring to view the monitoring status.

8.14.2.1 3

8.14.2.2 Single add monitored variable

Operation

Graphical Representation

Explanation

1. Click the "Single Add" button

image392

2. Select the variables you need to monitor, click "Complete, " and if the selected variable is an array, you can choose dimensions to monitor specific elements within the array.

image393

Note that dimension selection is only available when the variable is an array.

3. Open the Variable Monitoring in Status Monitoring to view the monitoring status.

image394

8.14.3 Monitored variables export/import

8.14.3.1 Monitored variables export

On the monitored variable list page, click the image269 button at the bottom left to enter the monitored variable export interface.

8.9.3.1 export

①

Monitored variable export target file (including path)

②

Monitored variable export list

③

Monitored variable export button

④

Variable filter box

Export steps: First, input or select the path for the monitored variable export target file in ①, and filter the variable by name in ④, if necessary. Then, check the variables to be exported in ②. Finally, click the button in ③ to execute the export, and the exported monitored variable file will be generated in the path specified in ①.

8.14.3.2 Monitored variable import

On the monitored variable list page, click the image271 button at the bottom left to enter the monitored variable import interface.

8.9.3.2 import

①

Monitored variable import file

②

Monitored variable import option, which is the strategy for handling entry conflict

③

Monitored variable import entry

④

Monitored variable import button

⑤

Variable filter box

Import steps: First, select the monitored variable file to be imported in ①. Then, select the conflict handling strategy in ② and the variables to be imported in ③. Finally, click the button in ④ to execute the import, and the selected variables will be imported locally.